all:
imx51,wince6.0 R3,WCE600_11.04.02_ER.
I build nk.nb0,it can work good.but i add a *.exe file to image,it can not jump to image as follow logs.
INFO: Using device name: 'MX5165535'
INFO: Reading NK image to SDHC (please wait)...
INFO: dwActualLength = [0x2339034]
INFO: Copying NK image to RAM address 0xa0200000
INFO: Read is 1% complete
INFO: Read is 2% complete
INFO: Read is 3% complete
INFO: Read is 4% complete
INFO: Read is 5% complete
INFO: Read is 6% complete
INFO: Read is 7% complete
INFO: Read is 8% complete
INFO: Read is 9% complete
INFO: Read is 10% complete
INFO: Read is 11% complete
INFO: Read is 12% complete
INFO: Read is 13% complete
INFO: Read is 14% complete
INFO: Read is 15% complete
INFO: Read is 16% complete
INFO: Read is 17% complete
INFO: Read is 18% complete
INFO: Read is 19% complete
INFO: Read is 20% complete
INFO: Read is 21% complete
INFO: Read is 22% complete
INFO: Read is 23% complete
INFO: Read is 24% complete
INFO: Read is 25% complete
INFO: Read is 26% complete
INFO: Read is 27% complete
INFO: Read is 28% complete
INFO: Read is 29% complete
INFO: Read is 30% complete
INFO: Read is 31% complete
INFO: Read is 32% complete
INFO: Read is 33% complete
INFO: Read is 34% complete
INFO: Read is 35% complete
INFO: Read is 36% complete
INFO: Read is 37% complete
INFO: Read is 38% complete
INFO: Read is 39% complete
INFO: Read is 40% complete
INFO: Read is 41% complete
INFO: Read is 42% complete
INFO: Read is 43% complete
INFO: Read is 44% complete
INFO: Read is 45% complete
INFO: Read is 46% complete
INFO: Read is 47% complete
INFO: Read is 48% complete
INFO: Read is 49% complete
INFO: Read is 50% complete
INFO: Read is 51% complete
INFO: Read is 52% complete
INFO: Read is 53% complete
INFO: Read is 54% complete
INFO: Read is 55% complete
INFO: Read is 56% complete
INFO: Read is 57% complete
INFO: Read is 58% complete
INFO: Read is 59% complete
INFO: Read is 60% complete
INFO: Read is 61% complete
INFO: Read is 62% complete
INFO: Read is 63% complete
INFO: Read is 64% complete
INFO: Read is 65% complete
INFO: Read is 66% complete
INFO: Read is 67% complete
INFO: Read is 68% complete
INFO: Read is 69% complete
INFO: Read is 70% complete
INFO: Read is 71% complete
INFO: Read is 72% complete
INFO: Read is 73% complete
INFO: Read is 74% complete
INFO: Read is 75% complete
INFO: Read is 76% complete
INFO: Read is 77% complete
INFO: Read is 78% complete
INFO: Read is 79% complete
INFO: Read is 80% complete
INFO: Read is 81% complete
INFO: Read is 82% complete
INFO: Read is 83% complete
INFO: Read is 84% complete
INFO: Read is 85% complete
INFO: Read is 86% complete
INFO: Read is 87% complete
INFO: Read is 88% complete
INFO: Read is 89% complete
INFO: Read is 90% complete
INFO: Read is 91% complete
INFO: Read is 92% complete
INFO: Read is 93% complete
INFO: Read is 94% complete
INFO: Read is 95% complete
INFO: Read is 96% complete
INFO: Read is 97% complete
INFO: Read is 98% complete
INFO: Read is 99% complete
INFO: Read is 100% complete
INFO: Copy of NK completed successfully
Download successful! Jumping to image at 0x0 (physical 0x90200000)...
it stoped.
the attach file is my config.bib,and i add a line
GrestCfg.exe | $(_FLATRELEASEDIR)\GrestCfg.exe NK | U |
the grestcfg.exe is 149KB.
are someone give me some advances,thanks.
Original Attachment has been moved to: config.bib.zip
If the booting stop because of this grestcfg.exe, then obviously this is not a problem of i.mx51 or wince drivers. the problem is in this grestcfg.exe. What I can suggest you is to debug this grestcfg.exe. :smileyhappy:
Hi jjimmychan:
I can not find why the system stop.
I do not modifty anything but rebuild and clean sysgen,the nk.nb0 can work good.
But when i modifty locale to chianese(simplified),after build,it stoped as the same msg.