Implement MIC on m33 on iMX8ULP-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implement MIC on m33 on iMX8ULP-EVK

262 Views
dhruvinrajpura
Contributor II

I am using imx8ulp_evk9 
https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-developm...

In this there is 2 portion 1 is a53 and another is m33, I want to test mic audio on m33 side for that I have mic : IM69D120V01XTSA1
So I want to record audio via mic and it should play on inbuild 3.5 mm jack but I am not able to find any sample or any thread on that, Can anyone explain?

0 Kudos
Reply
3 Replies

240 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

 

You can use our MCUXpresso SDK builder and take a look on the PDM examples as a reference for your design. 

 

JorgeCas_0-1713891712028.png

Best regards.

0 Kudos
Reply

235 Views
dhruvinrajpura
Contributor II

Hey @JorgeCas 

I taken example evk9mimx8ulp_dsp_pdm_sai_cm33, and build binary of that and generated flash.bin as well, but when I upload flash.bin with serial bootmode and than I turned on dualboot mode I am not seeing logs on m33 console,

Steps I am following for generate flash.bin in imx-mkimage
make SOC=iMX8ULP REV=A2 flash_dualboot_m33_xip

than I am uploading generated flash.bin into board with serial bootmode and than turning on with dualboot mode.

0 Kudos
Reply

223 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

 

I suggest you take a look on the next post.

 

Best regards.

0 Kudos
Reply