Image turn right or turn left without PXP on i.MX RT117x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Image turn right or turn left without PXP on i.MX RT117x

Jump to solution
600 Views
scarletlee
Contributor III

Hi,

May I make image turn right or turn left without PXP function on i.MX RT117X.

Thanks.

Labels (1)
0 Kudos
1 Solution
593 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) May I make image turn right or turn left without PXP function on i.MX RT117X.
-- Yes, I think so, however, it needs the developers to figure out the algorithm to make it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
594 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) May I make image turn right or turn left without PXP function on i.MX RT117X.
-- Yes, I think so, however, it needs the developers to figure out the algorithm to make it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos