The IR receiver (P/N IRM-V538M3/TR1) implemented on i.MX8M mini EVK.
This module connect to GPIO1_IO13 of i.MX8MM. However, I could not find any description to use this module into iMX8MMEVKUG and latest Linux BSP documents (L4.14.98_2.0.0_ga)
How do I use this module with linux BSP?
I suppose NXP will support lIRC later. is it right?
Copy from iMX8MMEVKHUG.pdf.
Best Regards,
Kazuma Sasaki.
已解决! 转到解答。
Hi,
The IR Receiver on the i.MX8M Mini EVK board is intended for IR Remote Receiving. GPIO1_IO13 will be assigned as IO input, and will work with INT mechanism and internal Timer to decode different IR Remote protocol, such as RC-5, RC-6, ans so on. Normally, this code shall be built by customers themselves.
Have a nice day
Rita
Hi,
The IR Receiver on the i.MX8M Mini EVK board is intended for IR Remote Receiving. GPIO1_IO13 will be assigned as IO input, and will work with INT mechanism and internal Timer to decode different IR Remote protocol, such as RC-5, RC-6, ans so on. Normally, this code shall be built by customers themselves.
Have a nice day
Rita
Hi Rita,
I appreciate your support. I see.
NXP has already validated IR receiver? because, current schematics is here.
I think we need rework D709 to receive signals from U701.
Best Regards,
Kazuma Sasaki.