INNOSTICK6 NXP i.MX6ULL based Computer Board in a small form factor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

INNOSTICK6 NXP i.MX6ULL based Computer Board in a small form factor

690 次查看
weidongzhou
Contributor I

INNOSTICK6-2_560.jpg

Based on NXP/Freescale's i.MX6ULL ARM Cortex-A7 processor with up to 900MHz CPU Clock, the INNOSTICK 6 is a portable and easy-to-use computer which integrated with on board DDR3 memory and eMMC storage in a tiny form factor(80mmx42mm). The INNOSTICK 6 provides a variety of interfaces and connectivity options - all packaged at an optimized power, size and cost. The INNOSTICK 6 highly integrated connectivity includes Wi-Fi, Bluetooth/BLE, USB Host and OTG, Camera, LCD display with touch panel and serial interfaces.

ikbd3_560.jpg

标签 (2)
0 项奖励
回复
0 回复数