IMx93 uses lt9611 chip to convert MIPI into DSI without image display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMx93 uses lt9611 chip to convert MIPI into DSI without image display

Jump to solution
2,151 Views
MasterLu
Contributor II

We use lt9611 to convert MIPI DSI to HDMI,then make the following configuration in the kernel:

1.Configured DRM_ LONTIUM_ LT9611=y in defconfig

2.Configure lt9611 and mipi dsi definitions in the device tree

 

hdmi@39 {
compatible = "lontium,lt9611";
pinctrl-0 = <&pinctrl_9611>;
pinctrl-names = "default";
  vdd-supply = <&reg_vddio_1v8>;
  vcc-supply = <&reg_vdd_3v3>;

reg = <0x39>;
reset-gpios = <&at9555 9 GPIO_ACTIVE_HIGH>;
enable-gpios = <&at9555 13 GPIO_ACTIVE_HIGH>;
interrupts-extended = <&gpio3 23 IRQ_TYPE_EDGE_FALLING>;
      status = "okay";

ports {
#address-cells = <1>;
#size-cells = <0>;

hdmi_disp: port@0 {
reg = <0>;

lt9611_1_in: endpoint {
remote-endpoint = <&mipi_dsi_bridge1_out>;
};
};

port@2 {
reg = <2>;
lt9611_out: endpoint {
remote-endpoint = <&hdmi_con>;
};
};
};
};

&dsi {
status = "okay";
ports{
#address-cells = <1>;
#size-cells = <0>;

hdmi:port@1 {
reg = <1>;
mipi_dsi_bridge1_out: endpoint {
remote-endpoint = <&lt9611_1_in>;
};
};
};
};

 

At this point, the compiled image has the following error in the startup log:

 

[    1.787959] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/dsi@4ae10000 to encoder DSI-34: -517
[    1.798060] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_bind] *ERROR* failed to attach bridge: -517
[    1.808108] dw-mipi-dsi-imx 4ae10000.dsi: [drm:dw_mipi_dsi_imx_probe] *ERROR* failed to register component: -517


failed to find dsi host

 

 

Then I made a simple modification to the lt9611 driver

 

in lt9611_probe function,remove lt9611_attach_dsi
static int lt9611_probe(struct i2c_client *client,
			const struct i2c_device_id *id)
{
...
...
	i2c_set_clientdata(client, lt9611);

	lt9611->bridge.funcs = &lt9611_bridge_funcs;
	lt9611->bridge.of_node = client->dev.of_node;
	lt9611->bridge.ops = DRM_BRIDGE_OP_DETECT | DRM_BRIDGE_OP_EDID |
			     DRM_BRIDGE_OP_HPD | DRM_BRIDGE_OP_MODES;
	lt9611->bridge.type = DRM_MODE_CONNECTOR_HDMIA;

	drm_bridge_add(&lt9611->bridge);
	printk("%s start\n",__func__);
	/* Attach primary DSI */
	/*
	lt9611->dsi0 = lt9611_attach_dsi(lt9611, lt9611->dsi0_node);
	if (IS_ERR(lt9611->dsi0)) {
		ret = PTR_ERR(lt9611->dsi0);
		goto err_remove_bridge;
	}
*/
	/* Attach secondary DSI, if specified */


in lt9611_irq_thread_handler,add lt9611_attach_dsi when hdmi pluged in
static irqreturn_t lt9611_irq_thread_handler(int irq, void *dev_id)
{
...
...
	/* hpd changed high */
	if (irq_flag3 & 0x40) {
		dev_info(lt9611->dev, "hdmi cable connected\n");

		regmap_write(lt9611->regmap, 0x8207, 0x7f);
		regmap_write(lt9611->regmap, 0x8207, 0x3f);
		printk("attach to dsi\n");
		lt9611->dsi0 = lt9611_attach_dsi(lt9611, lt9611->dsi0_node);
		if(lt9611->dsi0){
			printk("success\n");
		}
	}

 

Successfully modified lt9611 and dsi attach through the above changes. Execute the modetest and fbset commands to see the following information

 

modetest
....
...
trying to open device 'imx-drm'...done
Encoders:
id      crtc    type    possible crtcs  possible clones
34      0       DSI     0x00000001      0x00000001

Connectors:
id      encoder status          name            size (mm)       modes   encoders
35      0       connected       HDMI-A-1        150x100         0       34
  props:
        1 EDID:
                flags: immutable blob
                blobs:

                value:
                        00ffffffffffff0030ae861001010101
                        22150103810f0a78eee5b5a355499927
                        135054afef0045c081c0818081808180
                        9500950fd1c0a1130040415819202c58
                        36009a560000001c000000fc004c454e
                        204c3139353077440a20000000fd0032
                        4c1e510e000a202020202020000000ff
                        0042333433323834350a2020202001ce
                        020321714e0607020315961112130414
                        051f90230907078301000065030c0010
                        008c0ad090204031200c405500b98821
                        000018011d8018711c1620582c2500b9
                        882100009e011d80d0721c1620102c25
                        80b9882100009e011d00bc52d01e20b8
                        285540b9882100001e023a80d072382d
                        40102c4580b9882100001e00000000d0
        2 DPMS:
                flags: enum
                enums: On=0 Standby=1 Suspend=2 Off=3
                value: 0
        5 link-status:
                flags: enum
                enums: Good=0 Bad=1
                value: 0
        6 non-desktop:
                flags: immutable range
                values: 0 1
                value: 0
        4 TILE:
                flags: immutable blob
                blobs:

                value:

CRTCs:
id      fb      pos     size
33      0       (0,0)   (0x0)
  #0  nan 0 0 0 0 0 0 0 0 0 flags: ; type: 
  props:
        24 VRR_ENABLED:
                flags: range
                values: 0 1
                value: 0

Planes:
id      crtc    fb      CRTC x,y        x,y     gamma size      possible crtcs
31      0       0       0,0             0,0     0               0x00000001
  formats: XR24 AR24 RG16 XB24 AB24 AR15 XR15
  props:
        8 type:
                flags: immutable enum
                enums: Overlay=0 Primary=1 Cursor=2
                value: 1
        32 zpos:
                flags: immutable range
                values: 0 0
                value: 0

Frame buffers:
id      size    pitch


fbset

root@imx93evk:~# fbset

mode "1920x1080"
    geometry 1920 1080 1920 1080 32
    timings 0 0 0 0 0 0 0
    accel true
    rgba 8/16,8/8,8/0,0/0
endmode

 

Even if I can see the above information, HDMI still has no image output. I hope everyone can give me some suggestions

 

0 Kudos
Reply
1 Solution
2,014 Views
MasterLu
Contributor II

I added an hdmi enable function in lontium-lt9611.c.

Now it can be displayed, but it can only be displayed 1920x1080@60Hz

static void lt9611_hdmi_out_enable(struct lt9611 *lt9611) //dsren
{
	struct reg_sequence reg_cfg[] = {
		{ 0x8123, 0x40 },

		{ 0x82de, 0x20 }, 
		{ 0x82de, 0xe0 },

		{ 0x8018, 0xdc },
		{ 0x8018, 0xfc },

		{ 0x8016, 0xf1 },
		{ 0x8016, 0xf3 },
		{ 0x8011, 0x5a },
		{ 0x8011, 0xfa },

		{ 0x8130, 0xea },

	};
	regmap_multi_reg_write(lt9611->regmap, reg_cfg, ARRAY_SIZE(reg_cfg));
	
}

 

Reading the edid appears normal

[   11.413892] lt9611_read_edid edid Loop[0]:00 ff ff ff ff ff ff 00 05 e3 90 27 62 1b 00 00 2b 1d 01 03 80 3c 22 78 2e 67 a5 a5 55 4d a2 27 
[   11.441616] 
[   11.467163] lt9611_read_edid edid Loop[1]:0e 50 54 bf ef 00 d1 c0 b3 00 95 00 81 80 81 40 81 c0 01 01 01 01 4d d0 00 a0 f0 70 3e 80 30 20 
[   11.477767] 
[   11.500529] lt9611_read_edid edid Loop[2]:35 00 55 50 21 00 00 1a a3 66 00 a0 f0 70 1f 80 30 20 35 00 55 50 21 00 00 1a 00 00 00 fc 00 55 
[   11.510886] 
[   11.532560] lt9611_read_edid edid Loop[3]:32 37 39 30 52 33 42 0a 20 20 20 20 00 00 00 fd 00 17 4b 1e a0 3c 00 0a 20 20 20 20 20 20 01 d9 
[   11.542882] 
[   11.568331] lt9611_read_edid edid Loop[4]:02 03 3e f1 4c 90 04 03 1f 13 01 12 5d 5e 5f 60 61 23 09 07 07 83 01 00 00 6d 03 0c 00 20 00 38 
[   11.578674] 
[   11.604081] lt9611_read_edid edid Loop[5]:3c 20 00 60 01 02 03 67 d8 5d c4 01 78 80 03 e3 05 e3 01 e3 0f 00 0c e6 06 07 01 53 53 00 56 5e 
[   11.614409] 
[   11.639822] lt9611_read_edid edid Loop[6]:00 a0 a0 a0 29 50 30 20 35 00 55 50 21 00 00 1e 02 3a 80 18 71 38 2d 40 58 2c 45 00 55 50 21 00 
[   11.650152] 
[   11.675581] lt9611_read_edid edid Loop[7]:00 1e 4d 6c 80 a0 70 70 3e 80 30 20 3a 00 55 50 21 00 00 1a 00 00 00 00 00 00 00 00 00 00 00 c7 
[   11.685914] 
[   11.700134] lt9611_get_edid_block 
[   11.704176] drm_helper_probe_add_cmdline_mode
[   11.704236] mode[1]: 1920 x 1080drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.708619] mode[2]: 1920 x 1080drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.717321] mode[3]: 1920 x 1080drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.726024] mode[4]: 720 x 576drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.734722] mode[5]: 720 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.743252] mode[6]: 720 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.751775] mode[7]: 640 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.760306] mode[8]: 640 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.768832] mode[9]: 640 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.777353] mode[10]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.785878] mode[11]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.797954] mode[12]: 2560 x 1440drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.810031] mode[13]: 1920 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.822116] mode[14]: 1680 x 1050drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.834207] mode[15]: 1440 x 900drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.846293] mode[16]: 1280 x 1024drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.858280] mode[17]: 1280 x 960drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.870354] mode[18]: 1280 x 720drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.882344] mode[19]: 800 x 600drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.894338] mode[20]: 800 x 600drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.906241] mode[21]: 640 x 480drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.918141] mode[22]: 640 x 480drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.930039] mode[23]: 640 x 480drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.941949] mode[24]: 720 x 400drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.953857] mode[25]: 1280 x 1024drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.965762] mode[26]: 1024 x 768drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.977836] mode[27]: 1024 x 768drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.989826] mode[28]: 1024 x 768drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.001823] mode[29]: 832 x 624drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.013816] mode[30]: 800 x 600drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.025859] mode[31]: 800 x 600drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.037774] mode[32]: 1280 x 720drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.049680] mode[33]: 1920 x 1080drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.061677] mode[34]: 1280 x 720drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.073754] mode[35]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.085744] mode[36]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.097819] mode[37]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.110008] mode[38]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.122105] mode[39]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.134190] mode[40]: 1280 x 720drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.146265] mode[41]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.158252] mode[42]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.170323] mode[43]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.182406] Modeline "3840x2160": 60 533250 3840 3888 3920 4000 2160 2163 2168 2222 0x48 0x9
[   12.202901] Not using 3840x2160 mode: ERROR
[   12.207083] Modeline "3840x2160": 30 262750 3840 3888 3920 4000 2160 2163 2168 2191 0x40 0x9
[   12.215513] Not using 3840x2160 mode: PANEL
[   12.219690] Modeline "2560x1440": 60 241500 2560 2608 2640 2720 1440 1443 1448 1481 0x40 0x5
[   12.228121] Not using 2560x1440 mode: BAD
[   12.232130] Modeline "1920x2160": 60 277250 1920 1968 2000 2080 2160 2163 2173 2222 0x40 0x9
[   12.240575] Not using 1920x2160 mode: BAD
[   12.244587] Modeline "1680x1050": 60 119000 1680 1728 1760 1840 1050 1053 1059 1080 0x40 0x9
[   12.253021] Not using 1680x1050 mode: BAD
[   12.257027] Modeline "1440x900": 60 88750 1440 1488 1520 1600 900 903 909 926 0x40 0x9
[   12.265056] Not using 1440x900 mode: BAD
[   12.268992] Modeline "1280x1024": 60 108000 1280 1328 1440 1688 1024 1025 1028 1066 0x40 0x5
[   12.277433] Not using 1280x1024 mode: BAD
[   12.281443] Modeline "1280x960": 60 108000 1280 1376 1488 1800 960 961 964 1000 0x40 0x5
[   12.289531] Not using 1280x960 mode: BAD
[   12.293453] Modeline "1280x720": 60 74250 1280 1390 1430 1650 720 725 730 750 0x40 0x5
[   12.301370] Not using 1280x720 mode: BAD
[   12.305307] Modeline "800x600": 60 40000 800 840 968 1056 600 601 605 628 0x40 0x5
[   12.312875] Not using 800x600 mode: BAD
[   12.316709] Modeline "800x600": 56 36000 800 824 896 1024 600 601 603 625 0x40 0x5
[   12.324278] Not using 800x600 mode: BAD
[   12.328101] Modeline "640x480": 75 31500 640 656 720 840 480 481 484 500 0x40 0xa
[   12.335581] Not using 640x480 mode: BAD
[   12.339413] Modeline "640x480": 73 31500 640 664 704 832 480 489 492 520 0x40 0xa
[   12.347004] Not using 640x480 mode: BAD
[   12.350857] Modeline "640x480": 67 30240 640 704 768 864 480 483 486 525 0x40 0xa
[   12.358344] Not using 640x480 mode: BAD
[   12.362185] Modeline "720x400": 70 28320 720 738 846 900 400 412 414 449 0x40 0x6
[   12.369669] Not using 720x400 mode: BAD
[   12.373506] Modeline "1280x1024": 75 135000 1280 1296 1440 1688 1024 1025 1028 1066 0x40 0x5
[   12.381938] Not using 1280x1024 mode: BAD
[   12.385944] Modeline "1024x768": 75 78750 1024 1040 1136 1312 768 769 772 800 0x40 0x5
[   12.393854] Not using 1024x768 mode: BAD
[   12.397774] Modeline "1024x768": 70 75000 1024 1048 1184 1328 768 771 777 806 0x40 0xa
[   12.405685] Not using 1024x768 mode: BAD
[   12.409603] Modeline "1024x768": 60 65000 1024 1048 1184 1344 768 771 777 806 0x40 0xa
[   12.417515] Not using 1024x768 mode: BAD
[   12.421438] Modeline "832x624": 75 57284 832 864 928 1152 624 625 628 667 0x40 0xa
[   12.429008] Not using 832x624 mode: BAD
[   12.432840] Modeline "800x600": 75 49500 800 816 896 1056 600 601 604 625 0x40 0x5
[   12.440403] Not using 800x600 mode: BAD
[   12.444235] Modeline "800x600": 72 50000 800 856 976 1040 600 637 643 666 0x40 0x5
[   12.451800] Not using 800x600 mode: BAD
[   12.455632] Modeline "1280x720": 60 74250 1280 1390 1430 1650 720 725 730 750 0x40 0x5
[   12.463544] Not using 1280x720 mode: BAD
[   12.467463] Modeline "1920x1080": 50 148500 1920 2448 2492 2640 1080 1084 1089 1125 0x40 0x5
[   12.475901] Not using 1920x1080 mode: BAD
[   12.479912] Modeline "1280x720": 50 74250 1280 1720 1760 1980 720 725 730 750 0x40 0x5
[   12.487832] Not using 1280x720 mode: BAD
[   12.491757] Modeline "3840x2160": 24 297000 3840 5116 5204 5500 2160 2168 2178 2250 0x40 0x5
[   12.500186] Not using 3840x2160 mode: BAD
[   12.504201] Modeline "3840x2160": 25 297000 3840 4896 4984 5280 2160 2168 2178 2250 0x40 0x5
[   12.512632] Not using 3840x2160 mode: BAD
[   12.516636] Modeline "3840x2160": 30 297000 3840 4016 4104 4400 2160 2168 2178 2250 0x40 0x5
[   12.525068] Not using 3840x2160 mode: PANEL
[   12.529248] Modeline "3840x2160": 50 594000 3840 4896 4984 5280 2160 2168 2178 2250 0x40 0x5
[   12.537678] Not using 3840x2160 mode: ERROR
[   12.541857] Modeline "3840x2160": 60 594000 3840 4016 4104 4400 2160 2168 2178 2250 0x40 0x5
[   12.550292] Not using 3840x2160 mode: ERROR
[   12.554476] Modeline "1280x720": 60 74176 1280 1390 1430 1650 720 725 730 750 0x40 0x5
[   12.562386] Not using 1280x720 mode: BAD
[   12.566306] Modeline "3840x2160": 24 296703 3840 5116 5204 5500 2160 2168 2178 2250 0x40 0x5
[   12.574736] Not using 3840x2160 mode: BAD
[   12.578742] Modeline "3840x2160": 30 296703 3840 4016 4104 4400 2160 2168 2178 2250 0x40 0x5
[   12.587173] Not using 3840x2160 mode: PANEL
[   12.591352] Modeline "3840x2160": 60 593407 3840 4016 4104 4400 2160 2168 2178 2250 0x40 0x5
[   12.599783] Not using 3840x2160 mode: ERROR
[   12.603969] Modeline "1920x1080": 60 148500 1920 2008 2052 2200 1080 1084 1089 1125 0x40 0x5
[   12.612407] Modeline "1920x1080": 60 148500 1920 2008 2052 2200 1080 1084 1089 1125 0x40 0x5
[   12.620839] Modeline "1920x1080": 60 148352 1920 2008 2052 2200 1080 1084 1089 1125 0x40 0x5
[   12.629277] Modeline "720x576": 50 27000 720 732 796 864 576 581 586 625 0x40 0xa
[   12.636761] Modeline "720x480": 60 27027 720 736 798 858 480 489 495 525 0x40 0xa
[   12.644244] Modeline "720x480": 60 27000 720 736 798 858 480 489 495 525 0x40 0xa
[   12.651724] Modeline "640x480": 60 25200 640 656 752 800 480 490 492 525 0x40 0xa
[   12.659202] Modeline "640x480": 60 25175 640 656 752 800 480 490 492 525 0x40 0xa
[   12.666683] Modeline "640x480": 60 25175 640 656 752 800 480 490 492 525 0x40 0xa

 

View solution in original post

0 Kudos
Reply
4 Replies
2,081 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You should add more log print in lt9611 driver.

0 Kudos
Reply
2,075 Views
MasterLu
Contributor II

Here are all the logs

0 Kudos
Reply
2,024 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The edid seem incorrect, there is no refresh rate information about HDMI, you can dump edid in driver:

[ 18.092789] lt9611_get_edid_block
[ 18.096128] [drm:update_display_info] Supported Monitor Refresh rate range is 0 Hz - 0 Hz
[ 18.096147] [drm:update_display_info] HDMI: DVI dual 0, max TMDS clock 0 kHz
[ 18.096169] [drm:update_display_info] Supported Monitor Refresh rate range is 0 Hz - 0 Hz
[ 18.096176] [drm:update_display_info] HDMI: DVI dual 0, max TMDS clock 0 kHz

0 Kudos
Reply
2,015 Views
MasterLu
Contributor II

I added an hdmi enable function in lontium-lt9611.c.

Now it can be displayed, but it can only be displayed 1920x1080@60Hz

static void lt9611_hdmi_out_enable(struct lt9611 *lt9611) //dsren
{
	struct reg_sequence reg_cfg[] = {
		{ 0x8123, 0x40 },

		{ 0x82de, 0x20 }, 
		{ 0x82de, 0xe0 },

		{ 0x8018, 0xdc },
		{ 0x8018, 0xfc },

		{ 0x8016, 0xf1 },
		{ 0x8016, 0xf3 },
		{ 0x8011, 0x5a },
		{ 0x8011, 0xfa },

		{ 0x8130, 0xea },

	};
	regmap_multi_reg_write(lt9611->regmap, reg_cfg, ARRAY_SIZE(reg_cfg));
	
}

 

Reading the edid appears normal

[   11.413892] lt9611_read_edid edid Loop[0]:00 ff ff ff ff ff ff 00 05 e3 90 27 62 1b 00 00 2b 1d 01 03 80 3c 22 78 2e 67 a5 a5 55 4d a2 27 
[   11.441616] 
[   11.467163] lt9611_read_edid edid Loop[1]:0e 50 54 bf ef 00 d1 c0 b3 00 95 00 81 80 81 40 81 c0 01 01 01 01 4d d0 00 a0 f0 70 3e 80 30 20 
[   11.477767] 
[   11.500529] lt9611_read_edid edid Loop[2]:35 00 55 50 21 00 00 1a a3 66 00 a0 f0 70 1f 80 30 20 35 00 55 50 21 00 00 1a 00 00 00 fc 00 55 
[   11.510886] 
[   11.532560] lt9611_read_edid edid Loop[3]:32 37 39 30 52 33 42 0a 20 20 20 20 00 00 00 fd 00 17 4b 1e a0 3c 00 0a 20 20 20 20 20 20 01 d9 
[   11.542882] 
[   11.568331] lt9611_read_edid edid Loop[4]:02 03 3e f1 4c 90 04 03 1f 13 01 12 5d 5e 5f 60 61 23 09 07 07 83 01 00 00 6d 03 0c 00 20 00 38 
[   11.578674] 
[   11.604081] lt9611_read_edid edid Loop[5]:3c 20 00 60 01 02 03 67 d8 5d c4 01 78 80 03 e3 05 e3 01 e3 0f 00 0c e6 06 07 01 53 53 00 56 5e 
[   11.614409] 
[   11.639822] lt9611_read_edid edid Loop[6]:00 a0 a0 a0 29 50 30 20 35 00 55 50 21 00 00 1e 02 3a 80 18 71 38 2d 40 58 2c 45 00 55 50 21 00 
[   11.650152] 
[   11.675581] lt9611_read_edid edid Loop[7]:00 1e 4d 6c 80 a0 70 70 3e 80 30 20 3a 00 55 50 21 00 00 1a 00 00 00 00 00 00 00 00 00 00 00 c7 
[   11.685914] 
[   11.700134] lt9611_get_edid_block 
[   11.704176] drm_helper_probe_add_cmdline_mode
[   11.704236] mode[1]: 1920 x 1080drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.708619] mode[2]: 1920 x 1080drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.717321] mode[3]: 1920 x 1080drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.726024] mode[4]: 720 x 576drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.734722] mode[5]: 720 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.743252] mode[6]: 720 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.751775] mode[7]: 640 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.760306] mode[8]: 640 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.768832] mode[9]: 640 x 480drm_mode_validate_pipeline drm_crtc_mode_valid !MODE_OK MODE_OK
[   11.777353] mode[10]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.785878] mode[11]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.797954] mode[12]: 2560 x 1440drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.810031] mode[13]: 1920 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.822116] mode[14]: 1680 x 1050drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.834207] mode[15]: 1440 x 900drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.846293] mode[16]: 1280 x 1024drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.858280] mode[17]: 1280 x 960drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.870354] mode[18]: 1280 x 720drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.882344] mode[19]: 800 x 600drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.894338] mode[20]: 800 x 600drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.906241] mode[21]: 640 x 480drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.918141] mode[22]: 640 x 480drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.930039] mode[23]: 640 x 480drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.941949] mode[24]: 720 x 400drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.953857] mode[25]: 1280 x 1024drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.965762] mode[26]: 1024 x 768drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.977836] mode[27]: 1024 x 768drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   11.989826] mode[28]: 1024 x 768drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.001823] mode[29]: 832 x 624drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.013816] mode[30]: 800 x 600drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.025859] mode[31]: 800 x 600drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.037774] mode[32]: 1280 x 720drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.049680] mode[33]: 1920 x 1080drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.061677] mode[34]: 1280 x 720drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.073754] mode[35]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.085744] mode[36]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.097819] mode[37]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.110008] mode[38]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.122105] mode[39]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.134190] mode[40]: 1280 x 720drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.146265] mode[41]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.158252] mode[42]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.170323] mode[43]: 3840 x 2160drm_mode_validate_pipeline drm_bridge_chain_mode_valid !MODE_OK drm_mode_validate_pipeline != MODE_OK
[   12.182406] Modeline "3840x2160": 60 533250 3840 3888 3920 4000 2160 2163 2168 2222 0x48 0x9
[   12.202901] Not using 3840x2160 mode: ERROR
[   12.207083] Modeline "3840x2160": 30 262750 3840 3888 3920 4000 2160 2163 2168 2191 0x40 0x9
[   12.215513] Not using 3840x2160 mode: PANEL
[   12.219690] Modeline "2560x1440": 60 241500 2560 2608 2640 2720 1440 1443 1448 1481 0x40 0x5
[   12.228121] Not using 2560x1440 mode: BAD
[   12.232130] Modeline "1920x2160": 60 277250 1920 1968 2000 2080 2160 2163 2173 2222 0x40 0x9
[   12.240575] Not using 1920x2160 mode: BAD
[   12.244587] Modeline "1680x1050": 60 119000 1680 1728 1760 1840 1050 1053 1059 1080 0x40 0x9
[   12.253021] Not using 1680x1050 mode: BAD
[   12.257027] Modeline "1440x900": 60 88750 1440 1488 1520 1600 900 903 909 926 0x40 0x9
[   12.265056] Not using 1440x900 mode: BAD
[   12.268992] Modeline "1280x1024": 60 108000 1280 1328 1440 1688 1024 1025 1028 1066 0x40 0x5
[   12.277433] Not using 1280x1024 mode: BAD
[   12.281443] Modeline "1280x960": 60 108000 1280 1376 1488 1800 960 961 964 1000 0x40 0x5
[   12.289531] Not using 1280x960 mode: BAD
[   12.293453] Modeline "1280x720": 60 74250 1280 1390 1430 1650 720 725 730 750 0x40 0x5
[   12.301370] Not using 1280x720 mode: BAD
[   12.305307] Modeline "800x600": 60 40000 800 840 968 1056 600 601 605 628 0x40 0x5
[   12.312875] Not using 800x600 mode: BAD
[   12.316709] Modeline "800x600": 56 36000 800 824 896 1024 600 601 603 625 0x40 0x5
[   12.324278] Not using 800x600 mode: BAD
[   12.328101] Modeline "640x480": 75 31500 640 656 720 840 480 481 484 500 0x40 0xa
[   12.335581] Not using 640x480 mode: BAD
[   12.339413] Modeline "640x480": 73 31500 640 664 704 832 480 489 492 520 0x40 0xa
[   12.347004] Not using 640x480 mode: BAD
[   12.350857] Modeline "640x480": 67 30240 640 704 768 864 480 483 486 525 0x40 0xa
[   12.358344] Not using 640x480 mode: BAD
[   12.362185] Modeline "720x400": 70 28320 720 738 846 900 400 412 414 449 0x40 0x6
[   12.369669] Not using 720x400 mode: BAD
[   12.373506] Modeline "1280x1024": 75 135000 1280 1296 1440 1688 1024 1025 1028 1066 0x40 0x5
[   12.381938] Not using 1280x1024 mode: BAD
[   12.385944] Modeline "1024x768": 75 78750 1024 1040 1136 1312 768 769 772 800 0x40 0x5
[   12.393854] Not using 1024x768 mode: BAD
[   12.397774] Modeline "1024x768": 70 75000 1024 1048 1184 1328 768 771 777 806 0x40 0xa
[   12.405685] Not using 1024x768 mode: BAD
[   12.409603] Modeline "1024x768": 60 65000 1024 1048 1184 1344 768 771 777 806 0x40 0xa
[   12.417515] Not using 1024x768 mode: BAD
[   12.421438] Modeline "832x624": 75 57284 832 864 928 1152 624 625 628 667 0x40 0xa
[   12.429008] Not using 832x624 mode: BAD
[   12.432840] Modeline "800x600": 75 49500 800 816 896 1056 600 601 604 625 0x40 0x5
[   12.440403] Not using 800x600 mode: BAD
[   12.444235] Modeline "800x600": 72 50000 800 856 976 1040 600 637 643 666 0x40 0x5
[   12.451800] Not using 800x600 mode: BAD
[   12.455632] Modeline "1280x720": 60 74250 1280 1390 1430 1650 720 725 730 750 0x40 0x5
[   12.463544] Not using 1280x720 mode: BAD
[   12.467463] Modeline "1920x1080": 50 148500 1920 2448 2492 2640 1080 1084 1089 1125 0x40 0x5
[   12.475901] Not using 1920x1080 mode: BAD
[   12.479912] Modeline "1280x720": 50 74250 1280 1720 1760 1980 720 725 730 750 0x40 0x5
[   12.487832] Not using 1280x720 mode: BAD
[   12.491757] Modeline "3840x2160": 24 297000 3840 5116 5204 5500 2160 2168 2178 2250 0x40 0x5
[   12.500186] Not using 3840x2160 mode: BAD
[   12.504201] Modeline "3840x2160": 25 297000 3840 4896 4984 5280 2160 2168 2178 2250 0x40 0x5
[   12.512632] Not using 3840x2160 mode: BAD
[   12.516636] Modeline "3840x2160": 30 297000 3840 4016 4104 4400 2160 2168 2178 2250 0x40 0x5
[   12.525068] Not using 3840x2160 mode: PANEL
[   12.529248] Modeline "3840x2160": 50 594000 3840 4896 4984 5280 2160 2168 2178 2250 0x40 0x5
[   12.537678] Not using 3840x2160 mode: ERROR
[   12.541857] Modeline "3840x2160": 60 594000 3840 4016 4104 4400 2160 2168 2178 2250 0x40 0x5
[   12.550292] Not using 3840x2160 mode: ERROR
[   12.554476] Modeline "1280x720": 60 74176 1280 1390 1430 1650 720 725 730 750 0x40 0x5
[   12.562386] Not using 1280x720 mode: BAD
[   12.566306] Modeline "3840x2160": 24 296703 3840 5116 5204 5500 2160 2168 2178 2250 0x40 0x5
[   12.574736] Not using 3840x2160 mode: BAD
[   12.578742] Modeline "3840x2160": 30 296703 3840 4016 4104 4400 2160 2168 2178 2250 0x40 0x5
[   12.587173] Not using 3840x2160 mode: PANEL
[   12.591352] Modeline "3840x2160": 60 593407 3840 4016 4104 4400 2160 2168 2178 2250 0x40 0x5
[   12.599783] Not using 3840x2160 mode: ERROR
[   12.603969] Modeline "1920x1080": 60 148500 1920 2008 2052 2200 1080 1084 1089 1125 0x40 0x5
[   12.612407] Modeline "1920x1080": 60 148500 1920 2008 2052 2200 1080 1084 1089 1125 0x40 0x5
[   12.620839] Modeline "1920x1080": 60 148352 1920 2008 2052 2200 1080 1084 1089 1125 0x40 0x5
[   12.629277] Modeline "720x576": 50 27000 720 732 796 864 576 581 586 625 0x40 0xa
[   12.636761] Modeline "720x480": 60 27027 720 736 798 858 480 489 495 525 0x40 0xa
[   12.644244] Modeline "720x480": 60 27000 720 736 798 858 480 489 495 525 0x40 0xa
[   12.651724] Modeline "640x480": 60 25200 640 656 752 800 480 490 492 525 0x40 0xa
[   12.659202] Modeline "640x480": 60 25175 640 656 752 800 480 490 492 525 0x40 0xa
[   12.666683] Modeline "640x480": 60 25175 640 656 752 800 480 490 492 525 0x40 0xa

 

0 Kudos
Reply