IMXRT1176 SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMXRT1176 SDRAM

442 次查看
Chethanbg
Contributor III

Hi,

We are developing Instrument cluster application for one of our client using RT1176 controller.

We interfaced Winbond SDRAM 8MB (W9864G6KH-6I).We designed PCB and doing board bringup activity.

Below 2 pins are interchanged

From MCU bank select BA0 is connected to SDRAM BA1

From MCU bank select BA1 is connected to SDRAM BA0

This will cause any issue in SDRAM configuration??if it is causing what configuration settings we should change in firmware?

 

Attached is the image of SDRAM sch

 

 

 

 

0 项奖励
回复
2 回复数

408 次查看
Chethanbg
Contributor III

Any update on above ticket raised?

0 项奖励
回复

388 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @Chethanbg ,

This is a tough question. We haven't such experience. But I have to say I can't find any reason to oppose it.

 

regards,

Jing

0 项奖励
回复