IMX93 DSI to HDMI with lt9611uxc probe error: Failed to read chip rev

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX93 DSI to HDMI with lt9611uxc probe error: Failed to read chip rev

57 Views
AlanWen
Contributor III

I'm porting the DSI driver with LT9611UXC chip on I2C_3, as the LT9611UXC chip setup the I2C_ADDR as LOW (0x56) and I setup the kernel device tree.

&lpi2c3 {
	#address-cells = <1>;
	#size-cells = <0>;
	clock-frequency = <400000>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_lpi2c3>;
	status = "okay";
	lt9611uxc@56 {
		compatible = "lontium,lt9611uxc";
		reg = <0x56>;
		reset-gpios = <&gpio3 26 GPIO_ACTIVE_HIGH>;
		clock = <&clk>;
		clock-name = "ref";
		status = "okay";
		
		ports {
			#address-cells = <1>;
			#size-cells = <0>;

			port@0 {
				reg = <0>;
				lt9611uxc: endpoint {
					remote-endpoint = <&dsi_out>;
				};
			};

	};
};

But I can't probe the device on I2C bus successfully with i2cdetect command

root@imx93evk:~# i2cdetect -y 2
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:                         -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- 2b -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- 44 -- -- -- -- -- -- -- -- -- -- --
50: -- UU -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

 

While showing up the driver probing dmesg as below, it seems to be some error occurred.

root@imx93evk:~# dmesg | grep lt9611
[    2.113028] lt9611uxc 2-0056: supply vdd not found, using dummy regulator
[    2.119888] lt9611uxc 2-0056: supply vcc not found, using dummy regulator
[    2.512663] lt9611uxc 2-0056: failed to read revision: -5
[    2.576579] lt9611uxc 2-0056: failed to read chip rev
[    2.581886] lt9611uxc: probe of 2-0056 failed with error -5
[    8.947112] Error: Driver 'lt9611uxc' is already registered, aborting...

 

I'm not familiar with this chip and thus do not understand the nature of the problem.
Maybe you guys could help me out ?

0 Kudos
1 Reply

38 Views
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello, 

 

Could you please share the schematics regarding to I2C3 and lt9611uxc?

 

BR,

--... ...--

Salas.

0 Kudos