IMX8QXP uses Q10.0.0_2.2.0_AUTO_SOURCE and requires NVP6324 driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX8QXP uses Q10.0.0_2.2.0_AUTO_SOURCE and requires NVP6324 driver

655 次查看
relax-wu
Contributor IV

The current project uses NVP6324, is there a corresponding driver patch?

0 项奖励
回复
2 回复数

644 次查看
igorpadykov
NXP Employee
NXP Employee

Hi relax-wu

 

please refer to below patch:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Nvp6324-driver-for-imx8qm/ta-p/1114616

 

Best regards
igor

0 项奖励
回复

634 次查看
relax-wu
Contributor IV

Hi

If the driver migration is successful and the hardware path is normal, is it tested through the camera application that comes with the system?

0 项奖励
回复