IMX8QXP DDR 3G TO 4G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8QXP DDR 3G TO 4G

1,667 Views
gravity_one
Contributor III

Hello,all

What changes do You need to make to upgrade DDR (3G) to 4G?

SCFW,UBOOT,KERNEL?

Is there any documentation for that?

Tks,

Best regards,

Grayli

0 Kudos
Reply
1 Reply

1,636 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wang

in uboot one can tweak #define PHYS_SDRAM parameter

imx8qxp_mek.h\configs\include - uboot-imx - i.MX U-Boot 

rin ddr test   i.MX 8/8X Family DDR Tools Release  

For scfw  copy the custom DDR CFG file to src/scfw_export_mx8qx_b0/platform/board/mx8qx_mek/dcd and build to the final SCFW. One can try to follow the steps:

1. copy custom CFG file to dcd directory

cp xxx.CFG src/scfw_export_mx8qx_b0/platform/board/mx8qx_mek/dcd

 2. 

make clean

 3.

make qx R=B0 B=mek DDR_CON=xxx

May be recommended first not use OpTee, refer to sect.5.6.10 OP-TEE enablement

i.MX Yocto Project User’s Guide

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply