IMX8QXP 2 x 1Gb Ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8QXP 2 x 1Gb Ethernet

93件の閲覧回数
Chethanbg
Contributor III

Dear NXP Team,

We are designing a custom SOM module using the IMX8QXP processor. We require two 1Gb Ethernet ports. According to the pin configuration of the MiMX8QX6AVLFZAC, the ENET interface pins B32 (ENET0_MDIO), D30 (ENET1_MDC), and F28 (ENET0_REFCLK_125M_25M) are shared between ENET0 and ENET1.

Can we connect these three pins to both Ethernet PHY ICs?

Below is the pin config tool image for your reference.

Chethanbg_0-1718878704413.png

Chethanbg_1-1718878731251.png

 

 

0 件の賞賛
1 返信

75件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes, but you have to create the proper driver to work with it since linux BSP and/or android BSP works with one ethernet.

 

Regards

0 件の賞賛