hi sir,
when i use uuu tool in windows to update android 9(which i compiled), there is one error happened at the beginning,log as follow:
>uuu D:\uuu\Windows\uuu-android-mx8qm-mek-emmc.lst
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.0-0-g194351b
Success 0 Failure 1
1/ 0 [ ]
1:31 1/ 0 [HID(W):LIBUSB_ERROR_IO ]SDPS:boot -f uuu-u-boot-imx8qm.imx
is there any suggestion?
This error can come up if you are trying to load the wrong file.
In my case, I was trying to load the wrong <bootloader> from my Yocto build. The wrong <bootloader> I tried was u-boot-imx8qxpmek.bin, and the correct <bootloader> was imx-boot-imx8qxpmek-sd.bin.
Double check you are attempting to load the right files as suggested by Lorenzo Giraudi!
Hi,
I also encountered this problem, how do you solve it?
Try to use admin mode when running uuu tool. On Windows "Run as adminstrator" when you open the cmd, under Linux try with sudo. Under Linux you have the possibility to define udev rules so you don't need sudo.
I checked the picture you posted, you don't use the correct command, pls unzip the L4.14.98_2.0.0_ga_images_MX8QXPMEK.zip, then put uuu.exe in the same folder, then use the command as below:
uuu.exe uuu.auto, you can find uuu.auto in the unzip folder with other demo images
hi,joan
I want to use UUU download SPI_FLASH_64MB.bin to Qspi flash.
SPI_FLASH_64MB.bin (include:uboot,nernel,dtb,),,,,
i use SD download SPI_FLASH_64MB.bin to QSPI flash ,system is sucessful startup when set QSPI mode
prove .bin file is ok.
BRS
grayli
Hi Joan,
We're using our i.MX8QX(PN:PIMX8QX6AVLFZAB) board designed by our hardware team.
And MfgTool v2.8 works on windows 10, SO our hardware & pin configure works.
But uuu always got HID(W):LIBUSB_ERROR_IO. I also tried lorenzo.giraudi@ideasandmotion.com 's solution: using ubuntu 18.04, but still got LIBUSB_ERROR_IO even using sudo.
Actually I was trying to load the file containing secoFw+SCUFW+uboot. I discovered that I got the error on linux when i was trying to load an invalid file. So LIB_USBERR_IO may be caused by trying to load wrong files.
I meet the same issue on v1.3.93 now. It has take 10 months at least after this thread posted. And there is no meanful response from NXP.
UUU is not ready for production as a replacement of MfgTool now.
But MfgTool development stopped, if not dead.
SAD.
i have the problem too.my uuu tools version is 1.2.91;
C:\usr\UUU_1.2.91\android_p9.0.0_2.1.0-auto-ga_image_8qmek> .\uuu_imx_android_flash.bat -f imx8qm -e
This script is validated with uuu 1.2.91 version, please align with this version.
dual bootloader is supported
dtbo is supported
dual slot is supported
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash spl-imx8qm.bin to the partition of bootloader0
generate lines to flash bootloader-imx8qm.img to the partition of bootloader_a
generate lines to flash dtbo-imx8qm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8qm.img to the partition of vbmeta_a
generate lines to flash bootloader-imx8qm.img to the partition of bootloader_b
generate lines to flash dtbo-imx8qm.img to the partition of dtbo_b
generate lines to flash boot.img to the partition of boot_b
generate lines to flash system.img to the partition of system_b
generate lines to flash vendor.img to the partition of vendor_b
generate lines to flash vbmeta-imx8qm.img to the partition of vbmeta_b
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.2.91-0-g3799f4d
Success 0 Failure 1
1:3 1/ 1 [HID(R):LIBUSB_ERROR_IO ] SDPS: boot -f u-boot-imx8qm-mek-uuu.imx.link