Hi,
IMX8QM-MEK + Android 11 Automotive
I am getting following build error with modified kernel defconfig,
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:74] Fetch 'out/target/product/mek_8q/system/etc/vintf/compatibility_matrix.2.xml': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:84] List 'out/target/product/mek_8q/system_ext/etc/vintf/': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:74] Fetch 'out/target/product/mek_8q/system_ext/etc/vintf/manifest.xml': SUCCESS
checkvintf I 08-09 18:33:41 231 231 check_vintf.cpp:84] List 'out/target/product/mek_8q/product/etc/vintf/': No such file or directory
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] files are incompatible: Runtime info and framework compatibility matrix are incompatible: No compatible kernel requirement found (kernel FCM version = 5).
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] For kernel requirements at matrix level 5, Missing config CONFIG_SHADOW_CALL_STACK
checkvintf E 08-09 18:33:41 231 231 check_vintf.cpp:554] : Success
INCOMPATIBLE
[ 99% 768/771] Installed file list: out/target/product/mek_8q/installed-files-recovery.txt
[ 99% 769/771] Target vendor fs image: out/target/product/mek_8q/vendor.img
ninja: build stopped: subcommand failed.
18:33:51 ninja failed with: exit status 1^[[0;31m#### failed to build some targets (03:06 (mm:ss)) ####^[[00m
解決済! 解決策の投稿を見る。
Thank you @Bio_TICFSL for the reply.
This error occur with modified defconfig. I added my defconfig in automation_defconfig, with that there is no error.
Hello,
It looks like you need to add vintf driver by yourself or if you have driver is incompatible with the kernel version that android 12 have.
Regards
Thank you @Bio_TICFSL for the reply.
This error occur with modified defconfig. I added my defconfig in automation_defconfig, with that there is no error.