Hi,
I have an imx8qm-mek and I'm trying to stop the Cortex-M4 from the Linux system.
I followed the guide to compile the Linux image ( v. 5.15.32_2.0.0 ) using Yocto and I copied the resulting image on the microSD.
I also read the documentation about the Asymmetric Multi-Processing Application Processors.
When I execute the command:
echo stop > /sys/class/remoteproc/remoteproc1/state
I get the following error:
[ 273.961402] imx-rproc imx8qm_cm4@0: Failed to stop M4!
[ 273.966937] remoteproc remoteproc1: can't stop rproc: -13
Does anybody know which is the correct way to stop it?
Hi,
I tried the images that you share with me by email but they get me the same error message.