[IMX8MP] HDMI audio - no sound

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[IMX8MP] HDMI audio - no sound

128 次查看
jjiimmyy
Contributor II

I am using the multmedia image for the IMX8MP EVK.

Image version LF_v6.6.3-1.0.0_images_IMX8MPEVK.zip.

When playing wave file to HDMI audio output, I cannot hear sound.

root@imx8mpevk:/# aplay -Dplughw:1,0 /usr/share/sounds/alsa/Front_Center.wav
Playing WAVE '/usr/share/sounds/alsa/Front_Center.wav' : Signed 16 bit Little Endian, Rate 48000 Hz, Mono

root@imx8mpevk:/# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: btscoaudio [bt-sco-audio], device 0: 30c20000.sai-bt-sco-pcm-wb bt-sco-pcm-wb-0 [30c20000.sai-bt-sco-pcm-wb bt-sco-pcm-wb-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 1: audiohdmi [audio-hdmi], device 0: i.MX HDMI i2s-hifi-0 [i.MX HDMI i2s-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 3: wm8960audio [wm8960-audio], device 0: HiFi wm8960-hifi-0 [HiFi wm8960-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 3: wm8960audio [wm8960-audio], device 1: HiFi-ASRC-FE (*) []
Subdevices: 1/1
Subdevice #0: subdevice #0
card 4: imxaudioxcvr [imx-audio-xcvr], device 0: XCVR PCM snd-soc-dummy-dai-0 [XCVR PCM snd-soc-dummy-dai-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
root@imx8mpevk:/#

0 项奖励
回复
1 回复

98 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Please try to unblank the HDMI screen. e.g. echo 0 > /sys/class/graphics/fb2/blank  (where fb2 is your hdmi screen).

If you are displaying something on screen, you don't need to unblank it. Otherwise, you need to unblank the screen before you play the audio.

 

You can run below command to keep it unblank after run the unblank command.

echo -ne "\033[9]" > /dev/tty0

0 项奖励
回复