Hi,
We are trying to bring up the AW-CM276NF (88W8997) WiFi / BT combo module. We got the driver up and we could able to scan the wifi networks using command line:
iw dev mlan0 scan => getting the access points around us
iw dev mlan0 connect <access point name> => we could able to connect with the access point.
But when we are trying to use the Android UI, we found the following,
1. WiFi does not get powered on => keeps getting into power off stat
2. WiFi scan is not working, no AP list is populated
3. Could not able to connect with the any AP as well.
Please share your inputs on this.
Hi @VeeraH ,
I checked android 11.0.0_2.6.0 bsp source, driver is in the path:
~/android_11.0.0_2.6.0/vendor/nxp-opensource/nxp-mwifiex/mxm_wifiex/wlan_src
you can open it Makefile:
......
CONFIG_SD8997=y
CONFIG_USB8997=n
......
8997 with SDIO interface has been supported by the driver. It means that you don't neet to do any porting work.
it means that default android bsp should support it.
it only needs wifi module is on your board.
According to your logs, wifi driver (mlan.ko & moal.ko) is not ready.
Regards,
weidong
Hi,
Please find herewith my current settings.
############################################################################
# Configuration Options
#############################################################################
# Multi-chipsets
CONFIG_SD8887=n
CONFIG_SD8897=n
CONFIG_USB8897=n
CONFIG_PCIE8897=n
CONFIG_SD8977=n
CONFIG_SD8978=n
CONFIG_USB8978=n
CONFIG_SD8997=y
CONFIG_USB8997=n
CONFIG_PCIE8997=y
CONFIG_SD8987=n
CONFIG_SD9097=n
CONFIG_USB9097=n
CONFIG_PCIE9097=n
CONFIG_SD9098=n
CONFIG_USB9098=n
CONFIG_PCIE9098=n
Please share your inputs.
Hi,
I also tried with following. With only CONFIG_SD8997 is y, still same behavior is happening.
CONFIG_SD8997=y
CONFIG_USB8997=n
CONFIG_PCIE8997=n
Thanks,
Hariharan.V.
Hello @VeeraH ,
According to you logs, it seems that there are no wifi interfaces,such as wlan0 & wlan1.
wlan0 is STA , and WLAN1 is for hotspot.
Can you check if wifi driver has been build successfully in out directory?
-----------------------------------------------
weidong@ubuntu:~/android_11.0.0_2.6.0/out/target/product/mek_8q$ find -name mlan.ko
./vendor/lib/modules/mlan.ko
./obj/PACKAGING/depmod_VENDOR_intermediates/lib/modules/0.0/vendor/lib/modules/mlan.ko
./obj/PACKAGING/depmod_vendor_stripped_intermediates/mlan.ko
./obj/MXMWIFI_OBJ/mlan.ko
weidong@ubuntu:~/android_11.0.0_2.6.0/out/target/product/mek_8q$ find -name moal.ko
./vendor/lib/modules/moal.ko
./obj/PACKAGING/depmod_VENDOR_intermediates/lib/modules/0.0/vendor/lib/modules/moal.ko
./obj/PACKAGING/depmod_vendor_stripped_intermediates/moal.ko
./obj/MXMWIFI_OBJ/moal.ko
weidong@ubuntu:~/android_11.0.0_2.6.0/out/target/product/mek_8q$
---------------------------------------
Regards,
weidong
Hi,
NXP SDIO WiFi Driver creates mlan0 interface
but android framework expect and uses the wlan0 as STA.
After changing the information in the following files,
we could able to get the WiFi station is up and running on android UI as well.
Please share your inputs.
Hello @VeeraH ,
Yes , right. Android uses wlan0 / wlan1...
for nxp wifi driver, when you load it , you can set interface's name .
like: sta_name=wlan0, uap_name=wlan1 wfd_name=p2p ...
Regards,
weidong
Hello @VeeraH ,
I.MX8MP-EVK board supports 88W8997 with PCIe interface, WiFi is connected to M.2 interface on board.
Correspondingly, our default android 11 bsp also supports 88W8997 pcie module.
So suggest you check if there are something wrong with your porting procedure.
Regards,
weidong
We ported the 88W8997 with SDIO interface for WLAN and got the mlan0 interface on ifconfig.
using iw command, we could able to scan and connect using mlan0 interface.
we got mlan0 and p2p0 interface got created.
while debugging the logcat, we are getting following on WiFI ON using UI.
07-19 13:28:09.088 370 370 E WifiHAL : Timed out wating on Driver ready ...
07-19 13:28:09.088 370 370 E android.hardware.wifi@1.0-service: Failed or timed out awaiting driver ready
07-19 13:28:09.088 370 370 E android.hardware.wifi@1.0-service: Failed to start legacy HAL: TIMED_OUT
07-19 13:28:09.089 552 635 E HalDevMgr: executeChipReconfiguration: configureChip error: 9 (, timed out)
07-19 13:28:09.089 552 635 E WifiVendorHal: Failed to create STA iface
07-19 13:28:09.089 552 635 E WifiNative: Failed to create iface in vendor HAL
07-19 13:28:09.089 552 635 E WifiClientModeManager: Failed to create ClientInterface. Sit in Idle
wifi related configuration settings are fine as below,
wifi.interface => mlan0
wifi.direct.interface => p2p0
Please share your inputs
HI
how did you able to reslove this issue?
even i have same trace logs
Hi VeeraH! I have a problem,The development board I use is imx8qm.my DTS follows:Can you provide your configuration file
&usdhc2 {
pinctrl-names = "default", "state_100mhz", "state_200mhz";
pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>;
pinctrl-1 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>;
pinctrl-2 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>;
bus-width = <4>;
cap-power-off-card;
keep-power-in-suspend;
vmmc-supply = <®_usdhc2_vmmc>;
mmc_pwrseq = <&usdhc2_pwrseq>;
cd-gpios = <&lsio_gpio3 14 GPIO_ACTIVE_LOW>;
wp-gpios = <&lsio_gpio3 20 GPIO_ACTIVE_HIGH>;
status = "okay";
#address-cells = <1>;
#size-cells = <0>;
mwifiex: wifi@1 {
compatible = "marvell,sd8997";
reg = <1>;
};
};