IMX8MM - IOMUXC_SAI2_RXC_UART1_TX on pad AB22 fails.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX8MM - IOMUXC_SAI2_RXC_UART1_TX on pad AB22 fails.

跳至解决方案
966 次查看
Noel_V
Contributor III

Hello,

CPU : IMX8MM,

Using/building : linux-imx_4.14.98_2.3.0. 

HARDWARE: custom PCB design.

 

 

I'm trying to re-route uart1 and uart2 to  SAI2  SAI3 pads but for some reason, when trying to configure for example uart1 as below .


pinctrl_uart1: uart1grp {
fsl,pins = <
MX8MM_IOMUXC_SAI2_RXC_UART1_DTE_TX 0x140
MX8MM_IOMUXC_SAI2_RXFS_UART1_DTE_RX 0x140
>;
};

I don't see my tx-bytes at PAD-AB22 it seems as if this is still an RX-pin in stead of a TX-pin of the uart. ( when putting my oscilloscope on PAD-AC19 I see the TX coming out here and not on PAD-AB22.) 

 

For the 2nd uart I can send bytes  , but when connecting TX to RX I can't receive my own bytes ( it look is if there is no reception, while to oscilloscope proves that the bytes are arriving on the intended MX8MM_IOMUXC_SAI3_TXFS_UART2_DCE_RX pad)

pinctrl_uart2: uart2grp {
fsl,pins = <
MX8MM_IOMUXC_SAI3_TXC_UART2_DCE_TX 0x140
MX8MM_IOMUXC_SAI3_TXFS_UART2_DCE_RX 0x140
>;
};

Any hints ?

Thanks,

best regards

 

 

 

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Noel

 

>.. it seems as if this is still an RX-pin in stead of a TX-pin of the uart

 

in general this may be due to DCE/DTE described in Figure 16-10. UART external signals to

module signals routing with respect to DCE/DTE mode   i.MX 8M Mini Applications Processor Reference Manual

dts example :

https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/serial/f...

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
962 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Noel

 

>.. it seems as if this is still an RX-pin in stead of a TX-pin of the uart

 

in general this may be due to DCE/DTE described in Figure 16-10. UART external signals to

module signals routing with respect to DCE/DTE mode   i.MX 8M Mini Applications Processor Reference Manual

dts example :

https://source.codeaurora.org/external/imx/linux-imx/tree/Documentation/devicetree/bindings/serial/f...

 

Best regards
igor

0 项奖励
回复
957 次查看
Noel_V
Contributor III

Igor, 

 

You made may day  , iow SOLVED ! 

 

thanks for the hint ! 

Best Regards

Noel

 

 

 

0 项奖励
回复