Hello,
CPU : IMX8MM,
Using/building : linux-imx_4.14.98_2.3.0.
HARDWARE: custom PCB design.
I'm trying to re-route uart1 and uart2 to SAI2 SAI3 pads but for some reason, when trying to configure for example uart1 as below .
pinctrl_uart1: uart1grp {
fsl,pins = <
MX8MM_IOMUXC_SAI2_RXC_UART1_DTE_TX 0x140
MX8MM_IOMUXC_SAI2_RXFS_UART1_DTE_RX 0x140
>;
};
I don't see my tx-bytes at PAD-AB22 it seems as if this is still an RX-pin in stead of a TX-pin of the uart. ( when putting my oscilloscope on PAD-AC19 I see the TX coming out here and not on PAD-AB22.)
For the 2nd uart I can send bytes , but when connecting TX to RX I can't receive my own bytes ( it look is if there is no reception, while to oscilloscope proves that the bytes are arriving on the intended MX8MM_IOMUXC_SAI3_TXFS_UART2_DCE_RX pad)
pinctrl_uart2: uart2grp {
fsl,pins = <
MX8MM_IOMUXC_SAI3_TXC_UART2_DCE_TX 0x140
MX8MM_IOMUXC_SAI3_TXFS_UART2_DCE_RX 0x140
>;
};
Any hints ?
Thanks,
best regards
解決済! 解決策の投稿を見る。
Hi Noel
>.. it seems as if this is still an RX-pin in stead of a TX-pin of the uart
in general this may be due to DCE/DTE described in Figure 16-10. UART external signals to
module signals routing with respect to DCE/DTE mode i.MX 8M Mini Applications Processor Reference Manual
dts example :
Best regards
igor
Hi Noel
>.. it seems as if this is still an RX-pin in stead of a TX-pin of the uart
in general this may be due to DCE/DTE described in Figure 16-10. UART external signals to
module signals routing with respect to DCE/DTE mode i.MX 8M Mini Applications Processor Reference Manual
dts example :
Best regards
igor
Igor,
You made may day , iow SOLVED !
thanks for the hint !
Best Regards
Noel