IMX8MM DDR Stress Tool test stuck

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM DDR Stress Tool test stuck

1,576 Views
crcn
Contributor I

Hello.

I have a custom imx8mm board with a 512MB DDR4 (K4A4G165WE-BCTD).

I want to do the DDR stress test (following the User guide). For that, I configured the DDR4 parameters in the MX8M_Mini_DDR4_RPA_v20.xls

crcn_0-1675690209099.png

I did the calibration with these parameters in the Mscale DDR Tool:

crcn_1-1675690559218.png

 

But whhen I tried to do the Stress Test, it stuck's here:

Downloading file 'bin\ddr4_train1d_string_v201709.bin' ..Done

Downloading file 'bin\ddr4_train2d_string_v201709.bin' ..Done

Downloading file 'bin\ddr4_imem_1d_v201709.bin' ..Done

Downloading file 'bin\ddr4_dmem_1d_v201709.bin' ..Done

Downloading file 'bin\ddr4_imem_2d_v201709.bin' ..Done

Downloading file 'bin\ddr4_dmem_2d_v201709.bin' ..Done

Downloading IVT header...Done
Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done

Download is complete
Waiting for the target board boot...

===================hardware_init=====================
hardware_init exit

*************************************************************************

*************************************************************************

*************************************************************************
MX8 DDR Stress Test V3.30
Built on Nov 24 2021 13:30:14
*************************************************************************

Waiting for board configuration from PC-end...

--Set up the MMU and enable I and D cache--
- This is the Cortex-A53 core
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x93d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1122

- MMU and cache setup complete

*************************************************************************
ARM clock(CA53) rate: 1200MHz
DDR Clock: 1200MHz

============================================
DDR configuration
DDR type is DDR4
Data width: 16, bank num: 8
For DDR4, bank num is the total of 2 bank groups and 4 banks per group
Row size: 15, col size: 10
One chip select is used
Number of DDR controllers used on the SoC: 1
Density per chip select: 512MB
Density per controller is: 512MB
Total density detected on the board is: 512MB
============================================

MX8M-mini: Cortex-A53 is found

*************************************************************************

============ Step 1: DDRPHY Training... ============
---DDR 1D-Training @1200Mhz...
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of read DQ deskew training
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 1D-Training @533Mhz...
[Process] End of initialization
[Process] End of read enable training
[Process] End of fine write leveling
[Process] End of MPR read delay center optimization
[Process] End of Write Leveling coarse delay
[Process] End of write delay center optimization
[Process] End of read delay center optimization
[Process] End of max read latency training
[Result] PASS
---DDR 2D-Training @1200Mhz...
[Process] End of initialization
[Process] End of 2D read delay/voltage center optimization
[Process] End of 2D write delay/voltage center optimization
[Result] PASS

============ Step 2: DDR memory accessing... ============
Verifying DDR frequency point0@1200MHz.......Pass
Verifying DDR frequency point1@533MHz.......Pass
[Result] OK

============ Step 3: DDR parameters processing... ============
[Result] Done

Success: DDR Calibration completed!!!
DDR Stress Test Iteration 1
--------------------------------
--Running DDR test on region 1--
--------------------------------

t0.1: data is addr test

 

Can you help me? What I'm doing wrong?

Thanks.

 

Labels (1)
0 Kudos
4 Replies

1,391 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you share us the DDR datasheet to us?

0 Kudos

1,383 Views
crcn
Contributor I
0 Kudos

1,283 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Your configuration is right, how about your status in your side?

0 Kudos

1,539 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I will help check.

0 Kudos