iMXRT1052 Not boot from IS25WP064AJBLE nor Flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT1052 Not boot from IS25WP064AJBLE nor Flash

214 Views
Gianpaolo
Contributor I

I purchased an evkbimxrt1050 sch-38168 rev a1 evaluation board. I modified the resistors to use the IS25WP064AJBLE nor flash. I set SW7=0010. I compiled the firmware with the dcd and xip for nor flash. With the J-Link emulator the firmware works fine. once the emulator is disconnected, if I press the reset or power off and power on, it doesn't work anymore.

0 Kudos
1 Reply

189 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, but you have the same questions in another thread, I will be following your case in the other.

Best regards,
Pavel

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos