IMX8MM Crashes at smp: Bringing up secondary CPUs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8MM Crashes at smp: Bringing up secondary CPUs

1,184件の閲覧回数
santhosh2
Contributor IV

Hi,

our custom IMX8MM board was working fine with the same bootloader and Kernel (No change done) and suddenly Crashed at smp: Bringing up secondary CPUs,

Let me know whats the possible reason for the crash, Any voltage to issue or software issue?

Log is attached

Regards

Santhosh

0 件の賞賛
3 返答(返信)

1,116件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Santosh

one can try to reprogram image (as it can be corrupted for example due to sudden power off)

with GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Also may be recommended to retest memory with i.MX 8M Family DDR Tool Release 

please be aware of fix-derating-conflict-issue-L4.14.98_GA2.0.0.patch,

https://community.nxp.com/thread/525707 

its  software workaround has been integrated into the BSP

GA release imx_4.14.98_2.0.0 and latest  Register Programming Aid (RPA).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,116件の閲覧回数
santhosh2
Contributor IV

Hi igor,

I had tried re-flashing the board but still the same issue i am getting. I have tested all our application with 4.14.78 version, any other workaround ?

Since its difficult to go for L4.14.98 version

Note: I have tested with new board the image works fine 

0 件の賞賛

1,116件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Santosh

one can consider mechanical or ESD damage and try to resolder or change chip.

Best regards
igor

0 件の賞賛