IMX8MM Crashes at smp: Bringing up secondary CPUs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8MM Crashes at smp: Bringing up secondary CPUs

1,197 Views
santhosh2
Contributor IV

Hi,

our custom IMX8MM board was working fine with the same bootloader and Kernel (No change done) and suddenly Crashed at smp: Bringing up secondary CPUs,

Let me know whats the possible reason for the crash, Any voltage to issue or software issue?

Log is attached

Regards

Santhosh

0 Kudos
3 Replies

1,129 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santosh

one can try to reprogram image (as it can be corrupted for example due to sudden power off)

with GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Also may be recommended to retest memory with i.MX 8M Family DDR Tool Release 

please be aware of fix-derating-conflict-issue-L4.14.98_GA2.0.0.patch,

https://community.nxp.com/thread/525707 

its  software workaround has been integrated into the BSP

GA release imx_4.14.98_2.0.0 and latest  Register Programming Aid (RPA).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,129 Views
santhosh2
Contributor IV

Hi igor,

I had tried re-flashing the board but still the same issue i am getting. I have tested all our application with 4.14.78 version, any other workaround ?

Since its difficult to go for L4.14.98 version

Note: I have tested with new board the image works fine 

0 Kudos

1,129 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santosh

one can consider mechanical or ESD damage and try to resolder or change chip.

Best regards
igor

0 Kudos