IMX8M xtal bypass

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8M xtal bypass

Jump to solution
1,002 Views
GH
Contributor I

Hello,

I am designing a new board with the IMX8M on it and I'd like to use oscillators for the 25MHz and 27MHz inputs.  I see a hint that this is possible in the reference manual where it talks about bypass mode, but I don't see how to hook this up electrically.

1) Can I use an oscillator (1.8V output) as a clock for the IMX8M?

2) What exactly do I hook up to the XTAL1 and XTAL0 inputs for 25MHz and 27MHz?

3) Are there any other concerns with doing this? is there anything different that needs done in software for bootup?

 

Thanks!

0 Kudos
Reply
1 Solution
985 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi GH,

 

    I discussed your question with i.MX expert team, it is not recommended that you use OSC for i.MX8MQ.

    In addition, the amplitude of 25MHz and 27MHz clock is not 1.8V, BUT 1.1V.

 

Hope above information is helpful to you.

Have a nice day!

B.R,

Weidong

View solution in original post

0 Kudos
Reply
2 Replies
976 Views
GH
Contributor I

Weidong,

Thanks for the reply, I'll plan on using crystals instead.

have a good day!

0 Kudos
Reply
986 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi GH,

 

    I discussed your question with i.MX expert team, it is not recommended that you use OSC for i.MX8MQ.

    In addition, the amplitude of 25MHz and 27MHz clock is not 1.8V, BUT 1.1V.

 

Hope above information is helpful to you.

Have a nice day!

B.R,

Weidong

0 Kudos
Reply