IMX8DXL Support for DDR4 at 933MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX8DXL Support for DDR4 at 933MHz

131件の閲覧回数
chanks
Contributor I

Analysis for our board using the IMX8DXL shows that the board may have trouble supporting 1200MHz clock speeds for RAM but 933 MHz should be ok.

I was looking at the DDR4 version of the IMX8DXL DDR Register Programming Aid. The programming aid only supports frequencies of 800MHz and 1200MHz.  Is it possible to use DDR4 on the IMX8DXL at 933MHz? If so, can the programming aid be updated to support this?

 

 

ラベル(1)
0 件の賞賛
1 返信

109件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the reference manual, i.MX 8DualXLite and i.MX 8SoloXLite
embed a single DRAM 16-bit channel supporting LP-DDR4 and DDR3L memory types with inline ECC capability. and where did you find the DDR4 version, is it your typo?

0 件の賞賛