IMX8DXL DDR Stress Test Issue of USB recognition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8DXL DDR Stress Test Issue of USB recognition

569 Views
eric9
Contributor I

Hello,

I am trying to do DDR stress test using IMX8DXL-WEVK(Silicon b0) board  and mx8_ddr_stress_test_ER14_installation.exe

 

I connected 2 USB cables to USB_OTG2 port and USB_DEBUG.

After setting bootmode to USB serial download mode and power on.

They were recogized to "HID-compliant vender-defined device / USB Input device" and 4 USB Serial port on device manager 

eric9_0-1661395552217.pngeric9_1-1661395580617.png

I run(Run as administrator) DDR stress test SW (installed by mx8_ddr_stress_test_ER14_installation.exe) and tried to do ddr test.

But I encountered "ERROR: Can't open USB device!!!" error like below.

eric9_2-1661395830753.png

MX8_DDR_Tool_User_Guide describe supported ICs...

eric9_3-1661396163551.png

Is it different i.MX8DualX and i.MX8DualXLight (my IC is IMX8DXL)?
What should I check more?

 

 

 

 

 

 

 

 

 

0 Kudos
Reply
1 Reply

556 Views
jimmychan
NXP TechSupport
NXP TechSupport

Is it different i.MX8DualX and i.MX8DualXLight (my IC is IMX8DXL)?

Ans: They are different. Please contact the local FAE for the support of IMX8DXL DDR tool.

0 Kudos
Reply