IMX7D MII Device Tree - DP83640

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7D MII Device Tree - DP83640

3,036 Views
jameshall
Contributor I

Good Afternoon,

I currently have a custom board with an iMX7d (On an EA iMX7d uCOM SOM) connected to a DP8360 PHY via MII and I don't seem to be able to get comms working properly over the MII interface. The PHY is discovered and configured correctly over the MDIO bus and I can see sent TX packets in wireshark from UBOOT. Hoping I've missed something in the device tree,

Schematic,

jameshall_0-1628517748688.png

jameshall_1-1628517808541.png

Current Device Tree,

&fec1 {
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_enet1>;

	clocks = <&clks IMX7D_ENET_AXI_ROOT_CLK>,
		<&clks IMX7D_ENET_AXI_ROOT_CLK>,
		<&clks IMX7D_ENET1_TIME_ROOT_CLK>,
		<&clks IMX7D_PLL_ENET_MAIN_25M_CLK>;
	clock-names = "ipg", "ahb", "ptp", "enet_clk_ref";

	assigned-clocks = <&clks IMX7D_ENET1_TIME_ROOT_SRC>,
			  <&clks IMX7D_ENET1_TIME_ROOT_CLK>;
	assigned-clock-parents = <&clks IMX7D_PLL_ENET_MAIN_25M_CLK>;
	assigned-clock-rates = <0>, <100000000>;
	phy-mode = "mii";
	phy-handle = <&ethphy0>;
	fsl,magic-packet;
	status = "okay";

	mdio {
		#address-cells = <1>;
		#size-cells = <0>;

		ethphy0: ethernet-phy@0 {
			compatible = "ethernet-phy-ieee802.3-c22";
			reg = <1>;
		};
	};
};
pinctrl_enet1: enet1grp {
			fsl,pins = <

				MX7D_PAD_ENET1_COL__ENET1_COL		0x1
				MX7D_PAD_ENET1_CRS__ENET1_CRS		0x1

				MX7D_PAD_GPIO1_IO11__ENET1_MDC		0x3
				MX7D_PAD_GPIO1_IO10__ENET1_MDIO		0x3

				MX7D_PAD_ENET1_RX_CLK__ENET1_RX_CLK		0x1
				MX7D_PAD_ENET1_RGMII_RXC__ENET1_RX_ER	0x1

				MX7D_PAD_ENET1_TX_CLK__CCM_ENET_REF_CLK1	0x1
				
				MX7D_PAD_ENET1_RGMII_RD0__ENET1_RGMII_RD0	0x1
				MX7D_PAD_ENET1_RGMII_RD1__ENET1_RGMII_RD1	0x1
				MX7D_PAD_ENET1_RGMII_RD2__ENET1_RGMII_RD2	0x1
				MX7D_PAD_ENET1_RGMII_RD3__ENET1_RGMII_RD3	0x1

				MX7D_PAD_ENET1_RGMII_RX_CTL__ENET1_RGMII_RX_CTL 0x1
				MX7D_PAD_ENET1_RGMII_RXC__ENET1_RGMII_RXC 0x1

				MX7D_PAD_ENET1_RGMII_TD0__ENET1_RGMII_TD0	0x3
				MX7D_PAD_ENET1_RGMII_TD1__ENET1_RGMII_TD1	0x3
				MX7D_PAD_ENET1_RGMII_TD2__ENET1_RGMII_TD2	0x3
				MX7D_PAD_ENET1_RGMII_TD3__ENET1_RGMII_TD3	0x3
			>;
		};

 

Labels (2)
0 Kudos
Reply
2 Replies

3,029 Views
igorpadykov
NXP Employee
NXP Employee

Hi James

 

one can look at dts file on link

https://community.nxp.com/t5/i-MX-Processors/Does-iMX7D-ENET2-support-MII-interface/td-p/1297656

also recommended to check enet clock with oscilloscope, it is configured in uboot setup_fec()

register IOMUXC_GPR_GPR1, described in sect.8.2.4.2 GPR1 General Purpose Register (IOMUXC_GPR_GPR1)  i.MX 7Dual Applications Processor Reference Manual

https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx7dsabresd/mx7dsabresd.c?...

 

Best regards
igor

0 Kudos
Reply

3,014 Views
jameshall
Contributor I

Hi Igor,

Thanks for the link, I've rationalized my device tree (attached) against the one in the link you sent and updated my UBOOT to set the enet_clk to external,

 

clrsetbits_le32(&iomuxc_gpr_regs->gpr[1],
		 IOMUXC_GPR_GPR1_GPR_ENET1_CLK_DIR_MASK, IOMUXC_GPR_GPR1_GPR_ENET1_TX_CLK_SEL_MASK);

 

Still can't receive packets in UBOOT and now the PHY isn't coming up at all in Linux

James

0 Kudos
Reply