I got HAB event if I downloaded the FW through MFG Tool. I have tried to remove "0x00911000 0x2C 0x1C4 "u-boot.imx"" in csf file and got no HAB event.
Please advise how to download FW with MFG successfully with HAB.
Below is u-boot-imx.log
===============================================================
Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 565248 Bytes = 552.00 KiB = 0.54 MiB
Load Address: 877ff420
Entry Point: 87800000
HAB Blocks: 877ff400 00000000 00085c00
DCD Blocks: 00910000 0000002c 000001c4
===============================================================
Below is my csf file
===============================================================
[Header]
Version = 4.2
Hash Algorithm = sha256
Engine = ANY
Engine Configuration = 0
Certificate Format = X509
Signature Format = CMS
[Install SRK]
File = "../../crts/SRK_1_2_3_4_table.bin"
Source index = 0
[Install CSFK]
File = "../../crts/CSF1_1_sha256_2048_65537_v3_usr_crt.pem"
[Authenticate CSF]
[Install Key]
Verification index = 0
Target Index = 2
File = "../../crts/IMG1_1_sha256_2048_65537_v3_usr_crt.pem"
[Authenticate Data]
Verification index = 2
Blocks = 0x877FF400 0x000 0x85C00 "u-boot.imx", \
0x00911000 0x2C 0x1C4 "u-boot.imx"
===============================================================
Below is my steps:
1. ./mod_4_mfgtool.sh clear_dcd_addr u-boot.imx
2. /cst -o uboot_csf.bin -i uboot.csf
3. ./mod_4_mfgtool.sh set_dcd_addr u-boot.imx
4, cat u-boot.imx uboot_csf.bin > u-boot_signed.imx
5. Download u-boot_signed.imx with mfg tool
6. Power cycle again after download is finished
7. Enter u-boot
8. Type "hab_status"
9. below will be shown
HAB Configuration: 0xf0, HAB State: 0x66
--------- HAB Event 1 -----------------
event data:
0xdb 0x00 0x08 0x42 0x33 0x22 0x0a 0x00
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ADDRESS (0x22)
CTX = HAB_CTX_AUTHENTICATE (0x0A)
ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 2 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x00
0x00 0x00 0x00 0x20
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 3 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x2c
0x00 0x00 0x01 0xc4
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 4 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x7f 0xf4 0x20
0x00 0x00 0x00 0x01
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)
--------- HAB Event 5 -----------------
event data:
0xdb 0x00 0x14 0x42 0x33 0x0c 0xa0 0x00
0x00 0x00 0x00 0x00 0x87 0x80 0x00 0x00
0x00 0x00 0x00 0x04
STS = HAB_FAILURE (0x33)
RSN = HAB_INV_ASSERTION (0x0C)
CTX = HAB_CTX_ASSERT (0xA0)
ENG = HAB_ENG_ANY (0x00)
Hi Alice
one can try solution provided on
How to via MFG tool do security boot on the i.mx7d
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for your reply. We have signed uboot and zImage. Also, we did not found any problem in MFG tool so far. We got HAB event in uboot.
Do you mean I need to send request to get more information in your link provided?
Best regards,
Alice
Hi Alice
I sent you additional materials via mail.
If that will not help please proceed with extended support of
NXP Professional Services | NXP
Best regards
igor