IMX7 processor EIM interface hardware signal connection to communucate with an FPGA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7 processor EIM interface hardware signal connection to communucate with an FPGA

1,237 Views
Mailat
Contributor I

Hi,

I am using IMX7 processor and a Artix 7 series FPGA in my new design. I am planning to use the 16 bit multiplexed EIM interface to communicate between the IMX7 and FPGA. I am reffering the connection from OPOS6UL SP Interfaces description article in order to communicate between the IMX7 and FPGA. The article link is given below:

http://www.armadeus.org/wiki/index.php?title=OPOS6UL_SP_Interfaces_description

Is this the right way to do the EIM interface connection?

Or do you have any IMX7 specific design document for this application?

 

Thanks and Regards,

Vysakh

 

0 Kudos
Reply
1 Reply

1,208 Views
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Mailat,

I hope you are doing well.

Apologies for the delay in response.

Kindly refer to Section 9.7.2 External Signals of the i.MX7D Reference Manual for the EIM connection details.

Thanks & Regards,
Ritesh M Patel

0 Kudos
Reply