Hi,
I'm looking for any software support for a Cellular modem connected to IMX7- MCIMX7 SABRE platform using a Linux distribution. Anyone having any knowledge about what is already supported regarding API's and interfaces such as USB, PCIe to connect an external modem that could be accesses via an application or command line. Request for some suggestions for using GSM with my MY SABRE BOARD FOR a POC.
Thanks,
Sam
Thanks Igor..Ihave connected SIM800 GSM module and got the messaging working using AT Commands.
Thanks,
Syam
Hi Sam
one can look at boundary devices modem resources and try to use it for i.MX7
Cellular modems on i.MX6 boards under Ubuntu - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------