Hi community.
Our customer has below question.
Please advice me.
iMX6 Solo and Dual surface on heat radiation sheet and place the heat sink on .
Would you please disclose the load capacity of the iMX6.
解決済! 解決策の投稿を見る。
Hi Takashi
heat spreading and dissipation capabilities are described
in AN4579 i.MX 6 Series Thermal Management Guidelines,
in particular pay attention to Appendix D Heat Sink Selection
http://cache.nxp.com/files/32bit/doc/app_note/AN4579.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Takashi
heat spreading and dissipation capabilities are described
in AN4579 i.MX 6 Series Thermal Management Guidelines,
in particular pay attention to Appendix D Heat Sink Selection
http://cache.nxp.com/files/32bit/doc/app_note/AN4579.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Igor.
Thank you for your replay.
Although I got answer that there is no provision of the pressure load on the package of IMX6 in the previous question,
In simulation to i.MX6 compressive load 100N (10kg), 300N (30kg) and 1000N(100Kg) ,Can you determine no problem level in practical use ?
(I would like you to look at the presence or absence of occurrence of stress to the internal circuit as a determination material)
Thank you ,
Best Regards.
T.Takahashi