IMX6Solo and Dual surface load capacity .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Solo and Dual surface load capacity .

Jump to solution
518 Views
takashitakahash
Contributor III

Hi community.

Our customer has below question.

Please advice me.

iMX6 Solo and Dual surface on heat radiation sheet and place the heat sink on .

Would you please disclose the load capacity of the iMX6.

Labels (1)
0 Kudos
1 Solution
450 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

heat spreading and dissipation capabilities are described

in AN4579 i.MX 6 Series Thermal Management Guidelines,

in particular pay attention to Appendix D Heat Sink Selection

http://cache.nxp.com/files/32bit/doc/app_note/AN4579.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
451 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

heat spreading and dissipation capabilities are described

in AN4579 i.MX 6 Series Thermal Management Guidelines,

in particular pay attention to Appendix D Heat Sink Selection

http://cache.nxp.com/files/32bit/doc/app_note/AN4579.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
450 Views
takashitakahash
Contributor III

Dear Igor.

Thank you for your replay.

Although I got answer that there is no provision of the pressure load on the package of IMX6 in the previous question,

In simulation to i.MX6 compressive load 100N (10kg), 300N (30kg) and 1000N(100Kg) ,Can you determine no problem level in practical use ?

(I would like you to look at the presence or absence of occurrence of stress to the internal circuit as a determination material)

Thank you ,

Best Regards.

T.Takahashi

0 Kudos