Hello NXP Audio Experts,
We are using the iMX6 Solo for H.264 video on the VPU and
require about 25% of the 1GHz ARM for non-audio processing. We would like
an on-board audio codec with the following
prioritized considerations:
We would like 2-3 codec recommendations and why against
these 5 criteria along with their processing location and %utilization we can
expect on that processor (VPU, ARM, Neon).
As we are using H.264, we were unsure if AAC and MP3 are
considerations; someone suggested OPUS.
We appreciate your thoughts.
Thanks,
Swapna
Hi Swapna
one can use codecs which integrated on nxp reference boards:
please refer to attached Release Notes and Linux Manual
Chapter 28 Advanced Linux Sound Architecture (ALSA) System
on a Chip (ASoC) Sound Driver.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------