IMX6Solo/Ultralite/Solox Audio Codec Suggestion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Solo/Ultralite/Solox Audio Codec Suggestion

1,578 Views
swapnanannapane
Contributor I

Hello NXP Audio Experts,

We are using the iMX6 Solo for H.264 video on the VPU and
require about 25% of the 1GHz ARM for non-audio processing.  We would like
an on-board audio codec with the following
prioritized considerations:

  1. Stable and readily available minimizing
    integration time
  2. Non-optimized compression of office voice and
    non-CD quality stereo audio (any compression should reduce traffic sufficiently
    from 1Mbps per channel uncompressed)
  3. Fits on the
    ARM, the VPU, or the Neon coprocessor on the ARM
    (not sure if Neon’s purpose)
  4. Migratable to the IMX6 Ultralite or SoloX if the
    video requirement is removed
  5. Minimal-to-no license fee for <10,000 uses
    annually

We would like 2-3 codec recommendations and why against
these 5 criteria along with their processing location and %utilization we can
expect on that processor (VPU, ARM, Neon).

As we are using H.264, we were unsure if AAC and MP3 are
considerations; someone suggested OPUS.   

We appreciate your thoughts.

Thanks,

Swapna

Labels (3)
0 Kudos
Reply
1 Reply

1,371 Views
igorpadykov
NXP Employee
NXP Employee

Hi Swapna

one can use codecs which integrated on nxp reference boards:

please refer to attached Release Notes and Linux Manual

Chapter 28 Advanced Linux Sound Architecture (ALSA) System

on a Chip (ASoC) Sound Driver.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply