Hi,
I have a platform that is using the IMX6SDL SSI AUD3 INTERFACE to connect to a slave Device that support PCM data format. Can IMX6SDL SSI AUD3 be configured to support PCM data format in master mode?
Thanks,
Gus
You have to configure the SSI module for Normal mode, 1-bit wide early frame sync, 1 word per frame. There is no ready to use driver for such data format. For more information, check the corresponding chapter in the Reference Manual document.
Artur
Hi Artur,
When AUD3 is configure in master mode, does it support PCM audio data format?
The slave device is supporting the PCM audio data format, basically a single channel audio stream. We want to configure IMX6 AUD3 to run in 13bit or 16 bit linear PCM sample format. Can AUD3 Interface support this format?
Thanks again,
Gus
Yes, the AUD3 interface can be configured to operate in Master mode. For more information, please refer to the Chapter 16 "Digital Audio Multiplexer (AUDMUX)" and Chapter 61 "Synchronous Serial Interface (SSI)" of the i.MX6Solo/DualLite Reference Manual Rev.2 document, available on the NXP web site:
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Gus
SSI AUD3 can be used as master mode.
Please refer SSI clocking in i.MX6SDLRM.pdf.
Thanks
Saurabh