IMX6QuadPlus: VDD_HIGH_IN voltage range

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6QuadPlus: VDD_HIGH_IN voltage range

跳至解决方案
801 次查看
takayuki_ishii
Contributor IV

Hello community, 

Our customer ask us about reason of the specification change about VDD_SNVS_IN/VDD_HIGH_IN maximum

voltage range from 3.3V to 3.6V from imx6quad to imx6quadplus.

In EB810. it can show in section 18 Power.

By this document, it seems that reason is a max power consumption on VDD_SOC and NVDD_DRAM.

If both typical and maximum voltage are changed, I can understand.

But typical voltage keep a 3.0V.

Why does it change only maximum voltage range to 3.6V by max power consumption of VDD_SOC and

NVDD_DRAM?

Best regards,

Ishii.

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
719 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

it changed for more power design flexibility as allows more freedom

for input voltage and possible input voltage changes (instability) during power up

sequence. There is no special need to increase typical voltage as it increase power consumption.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
720 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

it changed for more power design flexibility as allows more freedom

for input voltage and possible input voltage changes (instability) during power up

sequence. There is no special need to increase typical voltage as it increase power consumption.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
719 次查看
takayuki_ishii
Contributor IV

Hello Igor

Thank you for your quick reply.

I understood why it was changed.

Best regards,

Ishii.

0 项奖励
回复