IMX6QuadPlus: VDD_HIGH_IN voltage range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6QuadPlus: VDD_HIGH_IN voltage range

Jump to solution
802 Views
takayuki_ishii
Contributor IV

Hello community, 

Our customer ask us about reason of the specification change about VDD_SNVS_IN/VDD_HIGH_IN maximum

voltage range from 3.3V to 3.6V from imx6quad to imx6quadplus.

In EB810. it can show in section 18 Power.

By this document, it seems that reason is a max power consumption on VDD_SOC and NVDD_DRAM.

If both typical and maximum voltage are changed, I can understand.

But typical voltage keep a 3.0V.

Why does it change only maximum voltage range to 3.6V by max power consumption of VDD_SOC and

NVDD_DRAM?

Best regards,

Ishii.

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
720 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

it changed for more power design flexibility as allows more freedom

for input voltage and possible input voltage changes (instability) during power up

sequence. There is no special need to increase typical voltage as it increase power consumption.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
721 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

it changed for more power design flexibility as allows more freedom

for input voltage and possible input voltage changes (instability) during power up

sequence. There is no special need to increase typical voltage as it increase power consumption.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
720 Views
takayuki_ishii
Contributor IV

Hello Igor

Thank you for your quick reply.

I understood why it was changed.

Best regards,

Ishii.

0 Kudos
Reply