IMX6Q gplay always in TASK_INTERRUPTIBLE stat!!!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q gplay always in TASK_INTERRUPTIBLE stat!!!

898 次查看
chenxiaoming
Contributor I

I run "gplay -r 1.7.mov maiken1.mpg 00004.mov weiduolila.mp4"  to play some videos by circle.  It plays well at first, but after about 10 hours, gplay falls into TASK_INTERRUPTIBLE stat and never wake up again. gplay indicate he is playing but actually he is stop.gplay shows some information as follow:

v4l2 alloc addr 0xc1000000

v4l2 alloc addr 0xc1400000

v4l2 alloc addr 0xc1800000

v4l2 alloc addr 0xc1c00000

v4l2 alloc addr 0xc2000000

v4l2 alloc addr 0xc2400000

v4l2 alloc addr 0xc2800000

v4l2 alloc addr 0xc2c00000

v4l2 alloc addr 0xc3000000

v4l2 alloc addr 0xc3400000

v4l2 alloc addr 0xc3800000

v4l2 alloc addr 0xc3c00000

full screen size:1920x1080

[V4L Update Display]: left=0, top=0, width=1920, height=1080

fsl_player_play()

get GST_MESSAGE_ELEMENT playbin2-stream-changed, uri=(string)file:///harddisk/weiduolila.mp4;

[Playing  (List Repeated)][Vol=01][00:41:03/00:42:17][fps:29]

[Playing  (List Repeated)][Vol=01][00:41:03/00:42:17][fps:29]

[Playing  (List Repeated)][Vol=01][00:41:03/00:42:17][fps:29]

[Playing  (List Repeated)][Vol=01][00:41:03/00:42:17][fps:29]

When I use "TOP" commamd,It shows:

Mem: 1814576K used, 22488K free, 0K shrd, 2588K buff, 1714348K cached

CPU:  0.0% usr  0.1% sys  0.0% nic 99.8% idle  0.0% io  0.0% irq  0.0% sirq

Load average: 4.00 4.01 4.05 1/78 3800

  PID  PPID USER     STAT   VSZ %VSZ CPU %CPU COMMAND

3393  3380 root     S     156m  8.7   2  0.1 ./gplay -r 1.7.mov maiken1.mpg 0000

3799  3380 root     R     2204  0.1   2  0.0 top

1574     2 root     SW       0  0.0   1  0.0 [kinteractiveup]

1427     2 root     SW       0  0.0   2  0.0 [kworker/2:1]

3380     1 root     S     2368  0.1   0  0.0 -/bin/sh

3390     1 root     S     2276  0.1   2  0.0 inetd

3381     1 root     S     2256  0.1   0  0.0 {rc_mxc.S} /bin/bash /etc/rc.d/rc_

    1     0 root     S     2200  0.1   1  0.0 init

3362     1 root     S     2188  0.1   0  0.0 /usr/sbin/dropbear

3386  3381 root     S     2068  0.1   2  0.0 sleep 100000

1586     1 root     S <   1756  0.1   1  0.0 udevd --daemon

1488     2 root     SW       0  0.0   0  0.0 [mmcqd/0]

    3     2 root     SW       0  0.0   0  0.0 [ksoftirqd/0]

    9     2 root     SW       0  0.0   1  0.0 [ksoftirqd/1]

   12     2 root     SW       0  0.0   2  0.0 [ksoftirqd/2]

   15     2 root     SW       0  0.0   3  0.0 [ksoftirqd/3]

    5     2 root     SW       0  0.0   2  0.0 [kworker/u:0]

3756     2 root     SW       0  0.0   0  0.0 [kworker/0:1]

  644     2 root     SW       0  0.0   2  0.0 [kswapd0]

It happens to me several times, If I ony run "gplay -r  00004.mov", gplay can run more than one day.It seems playing one video is  well.

But the way,my kernel is 3.0.35. And I have patched some patches to my kernel:

1. patch_v4l2_issue.zip( GStreamer crashing on i.MX6 (Boundary Devices Nitrogen6x)​),and I add [system("echo 3 > /proc/sys/vm/drop_caches")] to gplay before playing a new video.

2. 0009-ARM-imx-return-zero-in-case-next-event-gets-a-large-.patch \ 0026-ENGR00306257-1027-fix-system-hang-up-issue-caused-by.patch.txt

Can anyone give me some advise?

Thanks

Xiaoming

标签 (2)
0 项奖励
1 回复

408 次查看
art
NXP Employee
NXP Employee

This is the known issue with the L3.0.35 Linux BSP and it is caused by the memory fragmentation issue when allocating buffers for SDMA and IPU. There is still no good solution for it, so the better way is to migrate to the latest BSP version. The current version is L3.14.52.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励