We try to capture video from adv7181d
AUTODETECT CVBS IN NTSC/PAL/SECAM, 8-Bit 422 encoder:
What shuld be the IPUx_CSI0_SENS_CONF
We sets the IPUx_CSI0_SENS_CONF to 0x4004930
0x4004930
destination is IDMAC via SMFC | 16bit | YUV422 | YUV422
The problem
we didn't get any interrupts | BT656
Hi Itamar
adv7180 is supported in Sabre AI board:
imx6qdl-sabreauto.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel
driver description can be found in sect.6.1.7 V4L2 Capture Linux Manual
included in Linux 4.19.35_1.1.0 Documentation
Also may be useful TV-IN application note
https://community.nxp.com/docs/DOC-332679
15. i.MX Video Capture Driver — The Linux Kernel documentation
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------