IMX6Q boot failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
800件の閲覧回数
yacheng_zhang
Contributor I

Hi !

I am tring to design IMX6Q board.But something wrong.i set BOOT_MODE0 is 0 ,BOOT_MODE1 is 0,BOOT from fuses.It  can be boot success.(But there is actually mistake,i meant to internal boot Mode).

so i change boot setting,BOOT_MODE0 is 1,BOOT_MODE1 is 0.but it does not boot success.

The general phenomenon is that after i set BOOT pin to boot from fuses(Boot success!),then i set BOOT pin to boot from internal Boot Mode,But the board can not boot properly.

so i wonder why.

                                                   thank you

                                                   Yacheng Zhang

 

 

ラベル(2)
0 件の賞賛
返信
1 解決策
793件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

BOOT_MODE0 is 1,BOOT_MODE1 is 0   go to Serial download mode, details you can see in the RM:

2023 113.PNG

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
794件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

BOOT_MODE0 is 1,BOOT_MODE1 is 0   go to Serial download mode, details you can see in the RM:

2023 113.PNG

0 件の賞賛
返信
762件の閲覧回数
yacheng_zhang
Contributor I

     Sorry,There are mistakes in my word.In fact,i set BOOT_MODE0 is 0,BOOT_MODE1 is 1,It should be boot form internel,but it failed to boot.Then i try to set BOOT_MODE0 is 0,BOOT_MODE1 is 0,It should be boot from fuses,And it boot successfully.

So i want to know why failed boot from internel.

            thanks

           

 

 

0 件の賞賛
返信