IMX6Q Android6.0 Camera can't capture hight resolution picture well

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q Android6.0 Camera can't capture hight resolution picture well

738 Views
leavs
Contributor IV

Hi team,

I am using imx6q based hardware with Ov5640 module is connected to IPU1 CSI0 8bit [CSI0_DAT12  --- CSI0_DAT19] parallel camera interface.  Now, I can get Ov5640 to capture less then 1024x768 resolution pictures, but the resolution which is 1280x720 or higher don't work well. like follow picture.

pastedImage_1.png

I test follow resolution:

640x480  -- OK

1024x768 -- OK

1280*720 --  don't work well

1920x1080  -- don't work well

2592x1944 -- don't work well

I got follow kernel message:

Warnning:

=======

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001

Can you help me solve this problem??

Labels (1)
0 Kudos
4 Replies

594 Views
diegoadrian
NXP Employee
NXP Employee

Hi,

I am still working on this. I am having some problems with the camera app. I will update you as soon as I have an answer.

Best Regards,

Diego.

0 Kudos

594 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Have you tried using Android 7? I tested with that version and I did not have any problem with the camera. The images were taken without any problem.

Best regards,

Diego.

0 Kudos

594 Views
leavs
Contributor IV

Thanks for your reply.

Sorry, I don't work with Android7, there is only Android6.0 in my side.

0 Kudos

594 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Are you using as reference, our hardware setup and our drivers for the OV5640?

The CSI design is how we have on our reference board? Otherwise, we cannot guarantee anything.

Best Regards,

Diego.

0 Kudos