IMX6DQ6SDLHDG pdf

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6DQ6SDLHDG pdf

1,487 次查看
jburk
Contributor I

Regarding section 3.5.6 Four chips T topology routing examples: the pdf shows three layers of DDR3 routing, but there is clearly a fourth layer used that isn't shown. Would it be possible to get a screenshot of the missing layer?

0 项奖励
回复
1 回复

954 次查看
art
NXP Employee
NXP Employee

Generally, for all routing examples, refer to the i.MX6Q SABRE SD board PCB

design files, available as the i.MX6_SABRE_SDP_DESIGNFILES package on the NXP

web site (check the "Schematics" section):

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复