My kernel version 3.0.35 and android is 4.3, I need play back a sample rate of 22.05khz on the hdmi audio,but I find the driver didn't support the format, and when I'm forced to modify the driver, the sound will be distorted.
Hi ferdinand
there may be problem with 22.05khz on the hdmi audio since
there is no audio clock carried through the HDMI link, only the pixel clock is used.
Sect.33.4.6.1 CTS Calculation i.MX6DQ Reference Manual shows how it is produced
http://cache.nxp.com/files/soft_dev_tools/doc/support_info/iMX6DQPRM.pdf
Note, 22.05khz also should be provided from i.MX audio interface like SSI, ESAI
please refer to attached Linux Manual Chapter 28 Advanced Linux Sound Architecture
(ALSA) System on a Chip (ASoC) Sound Driver.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------