IMX6DP with isl79987 and LVDS in split mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DP with isl79987 and LVDS in split mode

Jump to solution
873 Views
vaudoitlaurent
Contributor IV

Hi,

we are working on a custom imx6DP board, with a LVDS screen (using 2 lvds bus in split mode), and an isl79987 video decoder.
Kernel is 4.19 from NXP, on which we have the isl79987 patch for the 4 channel feature.

For testing, we use gstreamer or the nxp test application, mxc_v4l_tvin.

When we display image from camera, we can see that the image is not perfect, some bloc of lines seems shifted from the previous one (cf picture).

If we force the isl79987 to display a test patter (on the same channel), then the image is correct (no block of lines shifted).


We made the same test on a Wandboard with imx6QP and a hdmi display, and we do not have the problem.


Would you have an idea on where to search for this problem?

Thans in advance for your help.

Regards

LaurentIMG_20200907_092030[1].jpg

1 Solution
856 Views
vaudoitlaurent
Contributor IV

Hi,

it seems the problems comes from the quartz used for the isl, which is not perfectly stable

Regards

Laurent

 

View solution in original post

2 Replies
849 Views
jamesbone
NXP TechSupport
NXP TechSupport

Great, thank you for sharing your solution

0 Kudos
Reply
857 Views
vaudoitlaurent
Contributor IV

Hi,

it seems the problems comes from the quartz used for the isl, which is not perfectly stable

Regards

Laurent