IMX6D - HDMI to VGA conversion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6D - HDMI to VGA conversion

695件の閲覧回数
ashasampathkuma
Contributor I

Hi all ,

we are working on a custom board based of imx6d and using Android M 6.0.1_1.0.1 BSP version.

Our board has an 7 inch display and uses LVDS interface.The LVDS display is working. We need to mirror the LVDS display contents to a VGA monitor.The screen mirroring is working for HDMI monitor but not for VGA.

We connected our board to  VGA monitor using HDMI to VGA adapter cable. The HDMI driver is unable to read the EDID data from monitor.

Whether imx hdmi driver supports VGA monitor?

Thanks,

Asha

ラベル(4)
0 件の賞賛
1 返信

491件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Asha

I am afraid imx hdmi driver does not support VGA monitor.

Only "true" HDMI monitor can send EDID information.

May be useful to look at similar description with DVI

DVI Support on i.MX6 boards - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛