IMX6 mixed EIM Voltages

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 mixed EIM Voltages

527 Views
nicholasschmidt
Contributor I

I need to add some 2.5 V GPIO pins to my IMX6 DualLite design, and for various reasons the only place I can put them is on EIM1 and 2. I need to leave EIM0 at 3.3 V. So I'd be powering EIM0 from 3.3 V and EIMs 1 and 2 from 2.5 V.

As far as I can tell this shouldn't be an issue for GPIO eFuse override at boot. Does anyone know whether this could be an issue?

Yes, I could just use a level translator, but...I can't.

Thanks,

Nick

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

446 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nick

no, there will no issues with powering EIM0 from 3.3 V and EIMs 1 and 2 from 2.5 V,

does not matter GPIO eFuse override at boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply