IMX6 mixed EIM Voltages

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 mixed EIM Voltages

490 次查看
nicholasschmidt
Contributor I

I need to add some 2.5 V GPIO pins to my IMX6 DualLite design, and for various reasons the only place I can put them is on EIM1 and 2. I need to leave EIM0 at 3.3 V. So I'd be powering EIM0 from 3.3 V and EIMs 1 and 2 from 2.5 V.

As far as I can tell this shouldn't be an issue for GPIO eFuse override at boot. Does anyone know whether this could be an issue?

Yes, I could just use a level translator, but...I can't.

Thanks,

Nick

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

409 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nick

no, there will no issues with powering EIM0 from 3.3 V and EIMs 1 and 2 from 2.5 V,

does not matter GPIO eFuse override at boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复