IMX6 mixed EIM Voltages

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 mixed EIM Voltages

591件の閲覧回数
nicholasschmidt
Contributor I

I need to add some 2.5 V GPIO pins to my IMX6 DualLite design, and for various reasons the only place I can put them is on EIM1 and 2. I need to leave EIM0 at 3.3 V. So I'd be powering EIM0 from 3.3 V and EIMs 1 and 2 from 2.5 V.

As far as I can tell this shouldn't be an issue for GPIO eFuse override at boot. Does anyone know whether this could be an issue?

Yes, I could just use a level translator, but...I can't.

Thanks,

Nick

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

510件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nick

no, there will no issues with powering EIM0 from 3.3 V and EIMs 1 and 2 from 2.5 V,

does not matter GPIO eFuse override at boot

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信