IMX6 VTT Termination with Pmic100 VREFDDR pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 VTT Termination with Pmic100 VREFDDR pin

692 Views
bastien
Contributor I

Hello,

I am working on imx6Q pcb board and I would like to use 4 DDR3 chips in fly-by topology.

In the 3.7§ DDR power recommendations of the Hardware Development Guide, NXP tells about DDR_VTT. I read articles and documentations which specify to use SW4 VTT mode.

I want to use the PMIC0100 chip in default mode.

1_ Does the VTT island can be provided by the VREFDDR pin (pmic)?

Also the number of decoupling capacitor is not clear.

2_ How many decoupling capacitors need to be placed on VTT island?

I saw Open Source project with decoupling capacitor between VTT and GND and between VTT and DDR_1.5V

3_ Did the last decoupling capacitor between VTT and DDR_1.5V is required ?

Hope someone could help me.

Best regards

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

642 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bastien

I sent example schematic for  4 DDR3 chips in fly-by topology via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply