IMX6 Solo not able to boot from EMMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 Solo not able to boot from EMMC

813 次查看
mahmood_md
Contributor I

imx6solo‌ uboot‌  emmc  boot‌

I am working on a custom imx6 solo board.

I am trying to write u-boot on the very first time to emmc, and able to write through DFU and UMS tool.

after successful written when I power off and change to boot mode(jumper)., I do not get any print or logs on the serial console.

with the same image, I am able to load on RAM itself and boot successfully.

Can you please help me to resolve this issue ASAP.

Your help is highly appreciated

Thanks,

Isharat

标签 (5)
标记 (4)
0 项奖励
回复
1 回复

734 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Isharat

issue may be related to signal integrity as described on

eMMC 8GB to 4GB - crash on linux (yocto) boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复