IMX6 Quad and Quad Plus 2 channel H/W encoding performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Quad and Quad Plus 2 channel H/W encoding performance

Jump to solution
1,587 Views
ivyliu
Contributor IV

Hi,

We want to try 2 channel H/W encoding simulaneously with IMX6 Quad or Quad Plus with 1080P or 720P.

We will use H.264.

Could someone tell me what is the highest 2 channel H/W encoding simulaneously performance for both Quad and Quad Plus with 1080P and 720P?

Can they both be 1080P@30fps?

Thanks and Best Regards,

Ivy

Labels (2)
0 Kudos
Reply
1 Solution
1,328 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

please check p.6 presentation for simultaneous encode performance

Q&A: MX6 VPU H.264 Dual Stream Encode Limits | NXP Community 

i.MX6Q and QP have the same vpu module.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

5 Replies
1,329 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

please check p.6 presentation for simultaneous encode performance

Q&A: MX6 VPU H.264 Dual Stream Encode Limits | NXP Community 

i.MX6Q and QP have the same vpu module.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,328 Views
ivyliu
Contributor IV

Hi Igor,

Thanks for your prompt reply.

Do you know what would be the maximum throughput when VPU is operating at 352 MHz?

Thanks and Best Regards,

Ivy

0 Kudos
Reply
1,328 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

below link may be useful

Memory Reserved on i.MX6 for VPU 

Best regards
igor

0 Kudos
Reply
1,328 Views
ivyliu
Contributor IV

Hi Igor,

Thank you for your reply.

I will try to decrease the size.

Do you know what would be the maximum throughput when VPU is operating at 352 MHz?

Thanks and Best Regards,

Ivy

0 Kudos
Reply
1,328 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivy

please check suggested presentation, it shows in brackets (vpu>300MHz)

Best regards
igor

0 Kudos
Reply